Ubuntu14.04 linux-runvbs.sh Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ubuntu14.04 linux-runvbs.sh Error

3,538 次查看
ohseohwan
Contributor I

Error in testing linux-runvbs.sh on ubuntu
What is the cause?

L4.1.15_2.1.0-ga_mfg-tools/mfgtools$ ./linux-runvbs.sh mfgtool2-yocto-mx-sabresd-emmc.vbs
mfgtool2-yocto-mx-sabresd-emmc.vbs
Executing: ./mfgtoolcli -l eMMC -s board=sabresd -s sxdtb=sdb -s mmc=3
Your Options:
board: sabresd
sxdtb: sdb
mmc: 3
Ready to flash.
init op Failed code# 24

标签 (3)
0 项奖励
回复
5 回复数

2,934 次查看
jimmychan
NXP TechSupport
NXP TechSupport

In the ucl2.xml, please try to remove the "    <STATE name="BootStrap" dev="MX6ULL" vid="15A2" pid="0080"/>"

0 项奖励
回复

2,934 次查看
ohseohwan
Contributor I

I modified the ucl2.xml file and tried again.

<CFG>
    <!--<STATE name="BootStrap" dev="MX6SL" vid="15A2" pid="0063"/>-->
    <!--<STATE name="BootStrap" dev="MX6SLL" vid="1FC9" pid="0128"/>-->
    <!--<STATE name="BootStrap" dev="MX6D" vid="15A2" pid="0061"/>-->
    <STATE name="BootStrap" dev="MX6Q" vid="15A2" pid="0054"/>
    <!--<STATE name="BootStrap" dev="MX6SX" vid="15A2" pid="0071"/>-->
    <!--<STATE name="BootStrap" dev="MX6UL" vid="15A2" pid="007D"/>-->
    <!--<STATE name="BootStrap" dev="MX7D" vid="15A2" pid="0076"/>-->
    <!--<STATE name="BootStrap" dev="MX6ULL" vid="15A2" pid="0080"/>-->
    <STATE name="Updater"   dev="MSC" vid="066F" pid="37FF"/>
  </CFG>

---------------------------------------

L4.1.15_2.1.0-ga_mfg-tools/mfgtools$ ./linux-runvbs.sh mfgtool2-yocto-mx-sabresd-sdcard-sd3.vbs
mfgtool2-yocto-mx-sabresd-sdcard-sd3.vbs
Executing: ./mfgtoolcli -l SDCard -s board=sabresd -s mmc=2 -s sxuboot=sabresd -s sxdtb=sdb
Your Options:
board: sabresd
mmc: 2
sxuboot: sabresd
sxdtb: sdb
Ready to flash.

----------------------------------------

I tried again and there is no response after Ready to flash.

0 项奖励
回复

2,934 次查看
jimmychan
NXP TechSupport
NXP TechSupport

You can check the MfgToolLibLog.txt to see where it stop.

0 项奖励
回复

2,934 次查看
ohseohwan
Contributor I

Thanks jimmychan 

The contents of MfgToolLibLog.txt are as follows.

-----------------------------------------------------------------

DLL version: 2.3.4
Mon Oct 16 20:13:29 2017
   Start new logging
ModuleID[2] LevelID[10]: address from XML 0x12000000

ModuleID[2] LevelID[10]: address from XML 0x80800000

ModuleID[2] LevelID[10]: address from XML 0x12C00000

ModuleID[2] LevelID[10]: address from XML 0x83800000

ModuleID[2] LevelID[10]: address from XML 0x18000000

ModuleID[2] LevelID[10]: address from XML 0x18000000

ModuleID[2] LevelID[10]: address from XML 0x83000000

ModuleID[2] LevelID[10]: address from XML 0x83000000

ModuleID[2] LevelID[10]: address from XML 0x83000000

ModuleID[2] LevelID[10]: address from XML 0x83000000

ModuleID[2] LevelID[10]: address from XML 0x83000000

ModuleID[2] LevelID[10]: address from XML 0x83000000

ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass

0 项奖励
回复

2,934 次查看
luwinbo
Contributor III

It's ready now, the last thing you have to do is power up your board.

0 项奖励
回复