Uboot serial console is not halting and uboot shell is not coming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot serial console is not halting and uboot shell is not coming

1,455 Views
srinivasaporam
Contributor II

Hi,

We have got wandboard quad board with us. When we are deploying some prebuilt images, tand powering on the board, it is booting correctly. for the prebuilt images we are using (uboot as well as kernel (Ubuntu trusty)).

Actually we would like deploy only uboot and see the boot messages in serial console (for our development purposes)

for this we have done following things:

1. We have connected USB to Serial Converter (USB is attached to my Ubuntu PC which is running minicom and serial is connected to wandboard quad's serial port. USB to serial converter cable is working fine. this we have checked using putty.

2. We have installed minicom in my ubuntu machine and set the serial port configutation (ttyUSB0,115200 etc).

3. start the minicom, by issuing command sudo minicom -D /dev/ttyUSB0 -o -w then minicom screen coming.

4. after deploying uboot to sd card, then kept sd card in sd card slot of wand board and powering on.

5. once powering on, we are hitting space bar in the keyboard which is connected to wandboard,

then messages are being displayed but uboot shell is not coming.

the messages are also not in english. Please find the message as below:

U-Boot 14.4 (un01204 212855 arhfcom

CP resal iM6Qe.a9M

  es u:Br Wdboa

: FS_SHC 0FSD:1

  ** Warin bC,sg faut nrmt

: se

Nt: C RE]rl

  Hi an ket soptobot 0

mis current device

Flenfond/ouEn.tt**Cckg i unvms e.

06bys ean26 ms(1MB/)

ooinfr mc 415yesrd n2s (4453i/s

eeim @10000 [x000 x6fa8] 

  #lateedev Tree blob 00 Booting usin et blb 1000 

artg nel.nplc100, nd1803f 

  

Itazig op ubysuset 

  Iitazggo sbssp 

  Itlzi co subyscpuacct 

Linuverson3.07-wand-armh.cm bldbu7)g rsn .2 Ubu/ao 82-9ut)) 1MPT Ju 32133TC204CP

M roesorfc09a revi RMv7, r=0387P: P/IT onlisngtace,VIT liing instrui ceMaheFrs

ce .6 u/Duai Decere) mdelWndod dbaedonFeca M6 ua 

a:A rerd5 MB t e000fto7ffvalocregion ovea. 

erpiy:E dsal,ataeaoc 

  RUm/pu@81fc00 3 r9d22 268 B1 onltiZnoreroiltyuino oalpaes 536

Krncmndle:nol=tym,100rot=/dev/mmcblk01 rw rotwid 

PID hash tleres40 rer,64bes 

Ie-cach hshte ntie 1372 or: 5288t)57 bt) 

  alote 53 yts f ecou 

lt cgupsalmemoryopi i dn' wneryrup 

Vil krnel memoy ay:erd0him 

  txt 000- 09d (00k00 0xf0000- 00000 ( 1MB (24M 

  ni: x8cba00- x8d080 280d0c00 00d 87 bsd690 0de0 (7kB 

  LU: l= de=3Oets, s,os

  

earc imleentin. 

  N_S:niqs16ch cntoleeabdlx0was,CHEI01000,UTR 03700 aceiz: 48 

  chdlo

CP ieniies .6 lo v .233,wraps eve 115 

nialiin crousbss vices02)pim:deaut:36 mim 31 

Initialig cgrouIti rpusysloIzgcgu subs prf: eti i uff hcy oCU0ha , sk mid800

ei ustaic forx06- 0x061 

  CPU1: otd ecnrpcsor 

CPU1: thread -1, cpu 1, sct,pr80001: Btsecdryprsr 

  CU r cp2, scke0mdr 80002P Btena

3 tre-cpu i 0000 

MToa o4osravte(22oMSCP: lCs)stred SCde 

em:naled xr:eaur fte hekmm4egs : 

o: unfnciona4rgs110.00Bec) 

DMApaload 56K ooaom heret llcainsUe DO as reset sourc 

vd1p1 80- 13 m 125V d3p: 00-> 15Vat300V d 

sycn e0imuc-pr egmapem 0x020e00-0e0037] egstred> 250mVa42 m 

syo2bc000.ocrlra[mxbc0-x01bfff rgitrehbaki: fu 5( ve ekpntn1 wtcpn rites. 

  hw-brea

kpoint: axmm tchpn szeisbys 

io ee sab<o0> mxq-intr 20e0000.omux iaid nclre 

  idt32x1 

  rid: nt3x2 13MBs 

ai: t2x4 12 M/srad6n328 Ms 

a6unnt2 4M 

1 25V P3 30 Vdh 

  _o_us 500mV 

vab ledi2coe:drer[mx113usiny susp method 

CIubtm niiaizd sinlegy esmemetd 

eia Lnu mdi ntfe: v00Lnuxvideotu ifacev20 bs 

  ppcor PAPIvr.reistre 

pscreSwer.5.36 Cpyrh 205207Rol oeti <ottlut 

  TPclck por rsere 

  mxipu 400.ip PUMC NMA

me1(1) (5), 56) 

  ix-pu3280MFCNORMAL mode: 1(0~1, B4,,F, 

xcip_ci22c00i_c: . I S hy eri s 33002a cmip_c2d0ip_i i PSI dirobd

I I drer odulloaded 

f21: ali Dtpde or rguatrdominze. 

  wih clocksce m_m1 ix6-pi 1c0i y linkcup 

  Pbrd b000:0p

_s000 ro bs esu [o 0x0-0x00s0::roo busreoc[mx1000-xef]c_b 00:0Nbu esoucfnf rtbu

ile bu -f 

pc00000:R:asged em x01000000-0x1f 

Trie16384 (orer: 5, 131072 byte)17bye00:0:B:m 1100-0ffr] 

Ha tls on(etlihe1684 n184 

  CP rrieedUDP hash table enties: 102 (: , t hsh etrs1 d

RP: gteednaed NI sk tanpot mdue.l famy1 

  PCRedud transpt mdue. 

RPCReiserdcpNv1 chnl asprtdle 

  w prfvetsenbld i MCrt- Uir7oursavibl 

prg-mmy parers 

B q rivr odl loaedm at tsuoe 

wbarfkllri25 wi-fk egtrekllanboill tdoad-rfkill.25: initie i p 

  wbordri kl.:nilie lutotcpwndoar-rkl l.bletoh-il gtd. 

  FSD

Dqtace as b enres14 (rr,0 be 

Keyypirlresred NFSRegstri thid_rlr ke pe 

usin PI eri .2) � 1-0R H,ngstre 

lok ayr SCSI generic (bsg) drir ved jor 29)ioscel orgteed 

  sel ealie egteed 

  i hurf

qesrd deaut)im-wi280emWEM rieriee 

xcsd_f .:eiermx dsadv him_dm 2e00.hiio Dtete HI onrol 10axa:0c1 

  c920VName - 2079m

i-iv2000ip: PUMF D HGROLUTION: 10,1), 5B(2~5), 5F(6,7) mx_sc_f.2:92x18hy,l ,8,18 vy,u 4,6 ixlk400 H 

oole ihngocoou fam fere-dm 200dm: o r asn, uinem 

  mxd e00.sma oadimwre1. 

m-sa20c00.dm:ntiid 

cosoetm0 eaedIO0x020 r=5 i aIM 

Id r1.1.00081[d iazvvae. MO 2ec0(iq ) i aI 

r d oad 

opmoul lde 

say XLs tae! 

  ag et, paallel scan dsale 

ci ai AC01300 32 slots 1 port Gs 1plptm odacihcfg ctsagpmdl pi s tccat 

  c0 cltfma

1:TA x M/13 ex200-0f] rt1 q 7libhy cetmiburoe e 2800.et ristr Cec eh_d UB .0nanc'

t ontlr(CI Direhci-pci EII pfmdrvubcr riser nw ntefae rier-sog 

_hdc _hrc.:oen' prggtchcchdc.: H st Controler 

ccci_c.: UB.0str, HC 10er,asignedbusnub 1 

h 10:.0 U hufn 

ub -01: 1ot tete 

sev /mousdvic cmf al mc 

  c-o:rer sl29023] usinla spdeho 

c-ore div[i292 si eg reumemeh 

mc_4l2_tt42_ut28 V2 deviceried ad1as tc 

i2-credrira11]sg leac ssndmh xv2opu vl2o.:4evcerestds vid7 

ccoe: drive a3110 ileac ume method 

im 2000.wWahg imr nl.ie6 wo0) 

md ri6 raltrstrefo level 6 d:rad1psaty giteedorleel1 

i5 petrstrd r i4 erai resef v 

ud: n gvenor ladder 

cpuidle: usi vrn enusdci Scre Dgit Htoreacder 

  dh:pigh(c rresma 

itf:DI patfo d O dre hlp 

dhc-d-x21980.sdccoud otgt t ig seedtt wrk on normal mode 

mm SDI norn 10dhc[900uscusig DMA 

  diehcim1400.sdcd ultrahi see sa, wrkonorald 

c vqruat n 

  1: DHIorlrn 19[2940.h sig A 

  dhisdc-m1900ushodno gur hieesta rkon norma mode 

m:noqcreultoron 

  hos desno suprt dngred-nlswitchasuin wre-ae 

  mmc: new high speed HC

ardaadresaaa 

mml mm0:aaaSU6148 GB ik o (Stat 0Ctl30) 

mm:SD ctlr 2000.h[19000shcsin AM 

  11:n wpeUS dc ne2si ci_hdrc 

cngnnowCIS tl0802tes) 

cqungnkn Itlx 7 t) Supl 8(besmmeugnon IStup 003yes) 

  mc qeungunowItplx tmm1: ewhispdDcdtdes1Gaco sio4.954mx_va10vai

Md t OrdteVArerpb 

c_rc 30.ac mc_rcreise 

  cp 24000v:VPitalized 

caa2000.dee ID= 0a1000 (a-524) 

2cm: uthc-hcbcaeaamshac-ac-acam 

a1000.aa tacsh2s-cam21000.caa: authecn-shs-cam20.ca: tc-m-5cde_ea 

  200.a:utcnhmc-

-c-secaa 

aam 210000cenchc-sha1-c-smaa 00m:uthbc-e-aa 

a am athnc-ch24c-es_e-a 

aa 2000caam: authencesn-hmch2c-des_ee-cam2000amauhec-ach25-c3ed-am 

  camha_eccamuhe

nc-mac-md5-cc--aa 

m21000.caam: authncsh-m100-cbc-des-caam 

cam 20000cam:uten-has256cbde-cama2000a thcha256-cbc-de-caamca200.caececaam 

  20000.

m100.m cr-escam 

  aa 000.aa:bescam mesa 

m 00.ca -3ecm 

plao2100.0reteg-amplfmam_ a_sme:-yteetesmachOK 

  lafom am:am_tt: -bteke te ath 

pto camsm ts 3-btek smachKpltfrmcamecvi.2: ecritolatioece hanls dwrwID esdrve ()

riKosa 

  p:ELDlS Etr Kyoa ves.aps0.sbchc.1/s/11/-1/p/pu 

d-ri 003:13:1001intidraw0 HID 1od E l UB rKeodon usbci_hdrc.1-1nt0 

usbor:egiteedewintfa irsbd 

si HD redrve 

c-or: iv cs28] ig ecyspd metd 

2cedrve[4288unley esmmhod 

  t0 00:g500reisonx1 

l5 00a ild 

0a100mVno001UsginerOinto VDDim-sgl500son2: g0 >0inkimx-sp sosi2:dii ->2040spfaio

  

xauiodmo-m2 dmhi- hdmi_audio.1mpinok 

  CP cuicrere 

:esteedprotcofmiy 

  p ble v6 

NET: Registered protocolfaily7K pdnroe rgisredVsupor v0:ileeo41 ricur3pat vint

reiedtakstseron1multnander 

nol [etc0]nabed 

  tnsoe nwkloginsre 

  v_c 0c034sns-tc-lp: setting system kto9--1 000UT

ASdilist: 

2i-iso #0:i6aba-stl00 

  Waiting rl dvic e vaib ereauteec 

d:fod'usrdue rdoudeect 

d:.utunOE.can 0an d dis.m:uor.. 4-fs (mmbl0p):udntoua et3duoftue comtiteEX-s cbl0p)odntosx2 u ncom 

  XT4f

smmbl1: ecvey pet 

X-(mckute flestmit odnul 

Vd rt(et4filysm) on ece 791 

vms:mn 

  enum: 30K(80a0 8d000 

  fr elinufs n /s/fs/selix: ch i irtryin:lou-tart-bde

ais 1) rmna t sas 

it pymoh-sarbrigmnressndd,reawin tu1 

itpmtupace 4)terinte wh st 

n:lmoth-upstart-bidminpros dedrpwnng 

  it uaahadires 4tmintedwihtaus 

it:lytust-brie maip rma wtstt 

init: plymouth-utt-bi minpress162 rn a outh-upstart-brn prces eded, respawning 

ov6_rad_egie :egEROR vl2tesav nond nit pmohupsarre prcesnd, esn 

  ae ntraceve o pe3.to:nusb py igured 

brmfmf_sdmdonl_fle Fito ut ra - 

  mfa: rcmdrc_dwnd_ra:doneme ldowldail 

  bma rcf_bus_s

tarbrmfrcmbu_iaied- 

  brcmfmac: brcmfsr_o gl i tspndnbrmfacc_sopredaa fed 

  cmarmfpsdo

_ro oroe aied-1.. 

*tating Populate /evilsyte[ K m obt4 

oig oplae evfiessm[ OK ] 

* StartgClantmp ityG O ] 

* StrtgPoula dli t/n7G[K ] * Sopi ack uttsrunig n a nir[7G[OK] 

oppnClan tmdiecory[74G[ 

*Strtn Sn sint ha irafesysemmounted[ ] 

*StingSialsynt a ll fesstmar m Srtig rgu ent itou 

* aiSnitteissar mou74G[ OK ] * S Mot filesstes oo[ OK] 

Saingevenod andernel evet aer4 OK] 

Soppg fuh r jo tto ls4[ K ]] 

*Si oa mlesfome/mus7[] K * Starting cold plugvic[ rn l itlecratn7G[ 

Sri bueohaOKagmet vi[7G[O] Stain era otsasOK 

Sarinyst lggngdaeon[7G[K 

  * So uslsh7[OK] 

* Srtg DDNS- emonK eplymtiu O 

*SarnRlo cps upn atiavaiano a rtqeua pa[ 

  Stppg ennevnttoindie pohsp[OK] 

*topinReoa cgvidaonoake se rme ueareputdO] 

toi cdugdece7G[K 

*trtgae de lgn ua uls4[ K]] 

tarn cnfurntwk vcesecuty[G[ OK ] 

dw3 dwc30.ut:o ub3phcofige 

Strtngonigreva ntwk viceG ] 

Srtg Bideoeeves nt us4[ ] 

Waingontrkcofutn.strt[G[OK

which language is this... is some thing wrong..how to get uboot shell.

Labels (4)
0 Kudos
Reply
0 Replies