Uboot crashes on 1 imx6ul board but not on another

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Uboot crashes on 1 imx6ul board but not on another

跳至解决方案
3,632 次查看
RayC
Contributor II

On one of our imx6ulevk like board (very similar to imx6ulevk), it crashes in u-boot immediately, on another board it boots normally to linux.

 

"Bad" board:

================================================== 

U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (Apr 07 2021 - 18:52:22 +0000)

CPU: i.MX6UL rev1.2 528 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
[0] lcdif@21c8000, video
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: Could not get PHY for FEC1: addr 1
Could not get PHY for FEC1: addr 1
Get shared mii bus on ethernet@2188000

Error: ethernet@2188000 address not set.
Get shared mii bus on ethernet@2188000
undefined instruction
pc : [<00000088>] lr : [<9ee99377>]
reloc pc : [<e898b088>] lr : [<87824377>]
sp : 9de6a7b8 ip : 00000020 fp : 00000017
r10: 9de91680 r9 : 9de72ed0 r8 : 9de744b8
r7 : 9de74458 r6 : 9f90b3c2 r5 : 00000004 r4 : 9de92588
r3 : 00000048 r2 : 00000006 r1 : 00000004 r0 : 9de92588
Flags: nzCv IRQs off FIQs off Mode SVC_32
Code: 00000000 00000000 00000012 20296328 (79706f43)
Resetting CPU ...

 

Good board with the same SD card:

==========================================================

U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (Apr 07 2021 - 18:52:22 +0000)

CPU: i.MX6UL rev1.2 528 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 35C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
[0] lcdif@21c8000, video
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: Could not get PHY for FEC1: addr 1
Could not get PHY for FEC1: addr 1
Get shared mii bus on ethernet@2188000

Warning: ethernet@2188000 using MAC address from ROM
eth0: ethernet@2188000
Fastboot: Normal
Normal Boot

....

 

Any ideas?

Thanks,

Ray

 

 

===================================

 

 

0 项奖励
回复
1 解答
3,577 次查看
RayC
Contributor II

Hi Igor,

Turned out the "bad" board can be "fixed" by fusing the OTP MAC address (Bank 4, words 2-4).

Also an older kernel and u-boot (version 4.9.88) boots up on all boards with or without a MAC address.

That led me to believe the new kernel and u-boot (version 5.4.70_2.3.0 Zeus) is sensitive to a 0:0:0:0:0:0 MAC address.

Maybe it's not really a crash but just an ASSERT in the new u-boot code? Has anyone else seen similar problems?

Thanks,

Ray  

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,529 次查看
vijayaragavansr
Contributor II

hi ,

 

Similar problem is faced in imx6ul board with latest kernel.

what is the solution?

Anyone found?

 

below is the UBoot Log

U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (May 31 2021 - 09:39:40 +0000)

CPU: i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 52C
Reset cause: POR
Board: MELANGE SYSTEMS - SBC
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
[0] lcdif@21c8000, video
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: Could not get PHY for FEC1: addr 1
Could not get PHY for FEC1: addr 1
Get shared mii bus on ethernet@2188000

Error: ethernet@2188000 address not set.
Get shared mii bus on ethernet@2188000
undefined instruction
pc : [<00000088>] lr : [<9ee99377>]
reloc pc : [<e898b088>] lr : [<87824377>]
sp : 9de6a7d8 ip : 00000020 fp : 00000017
r10: 9de91680 r9 : 9de72ed0 r8 : 9de744b8
r7 : 9de74458 r6 : 9f90b3c2 r5 : 00000004 r4 : 9de92588
r3 : 00000048 r2 : 00000006 r1 : 00000004 r0 : 9de92588
Flags: nzCv IRQs off FIQs off Mode SVC_32
Code: 00000000 00000000 00000011 20296328 (79706f43)
Resetting CPU ...

Thanks

Vijay

 

0 项奖励
回复
3,457 次查看
RayC
Contributor II

See my post below.

I worked around this by setting the MAC address fuse words (using an earlier u-boot and the u-boot "fuse" command.).

If someone has a u-boot patch that lets you boot up, please let us know.

0 项奖励
回复
3,628 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ray

 

had board passed ddr test, in general

reason may be poor soldering, one can try to replace chip.

 

Best regards
igor

0 项奖励
回复
3,578 次查看
RayC
Contributor II

Hi Igor,

Turned out the "bad" board can be "fixed" by fusing the OTP MAC address (Bank 4, words 2-4).

Also an older kernel and u-boot (version 4.9.88) boots up on all boards with or without a MAC address.

That led me to believe the new kernel and u-boot (version 5.4.70_2.3.0 Zeus) is sensitive to a 0:0:0:0:0:0 MAC address.

Maybe it's not really a crash but just an ASSERT in the new u-boot code? Has anyone else seen similar problems?

Thanks,

Ray  

0 项奖励
回复
3,610 次查看
RayC
Contributor II

Thank you, Igor.

Strangely, a much older image (4.9 kernel, 4.9 device tree) boots up even on the "bad" board.

Is it possible some (5.4.70 kernel) device tree setting may have caused this?

Since I am not very familiar with the processor, I am more than a little puzzled.

How do I read the "Code"?  All I can see is there's an invalid instruction. pc is at 88, I suppose this is very early on in u-boot.

 

Thanks,

Ray

 

 

undefined instruction
pc : [<00000088>] lr : [<9ee99377>]
reloc pc : [<e898b088>] lr : [<87824377>]
sp : 9de6a7b8 ip : 00000020 fp : 00000017
r10: 9de91680 r9 : 9de72ed0 r8 : 9de744b8
r7 : 9de74458 r6 : 9f90b3c2 r5 : 00000004 r4 : 9de92588
r3 : 00000048 r2 : 00000006 r1 : 00000004 r0 : 9de92588
Flags: nzCv IRQs off FIQs off Mode SVC_32
Code: 00000000 00000000 00000012 20296328 (79706f43)
Resetting CPU ...

 

0 项奖励
回复