Uboot UMS flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot UMS flashing

2,339 Views
Tanu_1827
Contributor I

Hello,

I am using iMX8DXL processor, UMS(USB Mass Storage) flashing is enabled in u boot and working as expected like partitions are get mounted in Linux pc ubuntu.

My question is this ums flasing is works in windows? if yes means how?

0 Kudos
Reply
7 Replies

2,298 Views
Tanu_1827
Contributor I

Hello @Manuel_Salas 

Flashed uboot ums enabled software and board is booting, stop at uboot 

Tanu_1827_0-1713846386674.png

Once command is executed successfully, eMMC partition 1 and 2 will get mounted to the ubuntu PC

In Ubuntu PC working as expected.

In windows is possible to flash through ums and can we see mounted partition in windows PC?

 

 

0 Kudos
Reply

2,264 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Tanu_1827 

 

Yes, I tested by my side and tehre is not problem, the operating system (Windows or Linux) will detect the board as USB Mass Storage.

 

Best regards.

 

Salas.

0 Kudos
Reply

2,209 Views
Tanushree
Contributor III

hello @Manuel_Salas 

Yes its detected as a USB. but in our case the partition is in ext4 filesystem which is not compatible on windows. its asking for a format the disk.

Regards,

Tanushree

0 Kudos
Reply

2,203 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Tanushree 

Of course Windows does not support EXT4 natively, you can install a driver for Windows called Ext2Fsd that will read and write EXT4 or a tool called Ext2Read.

 

I hope this can helps.

 

Best regards.

 

Salas.

0 Kudos
Reply

2,122 Views
Tanushree
Contributor III

UMS utility on Windows is blocked by a read-only mounted partition, when we use Ext2Fsd tool

0 Kudos
Reply

2,046 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,316 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Tanu_1827 

 

Could you please share the steps that you did to reproduce it in Linux and Windows PC host?

 

Best regards.

 

Salas.

0 Kudos
Reply