UVC Gadget Driver Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UVC Gadget Driver Issue

2,881件の閲覧回数
sunil_embex
Contributor I

Dear Team,

 

I am using IMX8M-Mini evk board and trying to configure usb uvc gadget  driver.

I followed this link: https://developer.ridgerun.com/wiki/index.php/How_to_use_the_UVC_gadget_driver_in_Linux

But I am not able to see any node in /sys/class/udc. 

Can you please help and do the needful.

Regards,

Sunilk

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,870件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the BSP version that you're working with?
Also, to which USB port are you using for your test?

Best regards,
Aldo.

0 件の賞賛
返信

2,836件の閲覧回数
sunil_embex
Contributor I

Hi Aldo,

Thanks for reply. I moved on the usb printer gadget driver and i am able to transfer data on default end points.

Further I have added two more endpoints and able to see in libusb output but not able to send/receive data so if you can help me to resolve this issue that would be really great help otherwise you can close the ticket.

Below is the driver

// SPDX-License-Identifier: GPL-2.0+
/*
* f_printer.c - USB printer function driver
*
* Copied from drivers/usb/gadget/legacy/printer.c,
* which was:
*
* printer.c -- Printer gadget driver
*
* Copyright (C) 2003-2005 David Brownell
* Copyright (C) 2006 Craig W. Nadler
*/

#include <linux/module.h>
#include <linux/kernel.h>
#include <linux/delay.h>
#include <linux/ioport.h>
#include <linux/sched.h>
#include <linux/slab.h>
#include <linux/mutex.h>
#include <linux/errno.h>
#include <linux/init.h>
#include <linux/idr.h>
#include <linux/timer.h>
#include <linux/list.h>
#include <linux/interrupt.h>
#include <linux/device.h>
#include <linux/moduleparam.h>
#include <linux/fs.h>
#include <linux/poll.h>
#include <linux/types.h>
#include <linux/ctype.h>
#include <linux/cdev.h>
#include <linux/kref.h>
#include <asm/byteorder.h>
#include <linux/io.h>
#include <linux/irq.h>
#include <linux/uaccess.h>
#include <asm/unaligned.h>
#include <linux/usb/ch9.h>
#include <linux/usb/composite.h>
#include <linux/usb/gadget.h>
#include <linux/usb/g_printer.h>
#include "u_printer.h"

#define PRINTER_MINORS 4
#define GET_DEVICE_ID 0
#define GET_PORT_STATUS 1
#define SOFT_RESET 2

#define DEFAULT_Q_LEN 10 /* same as legacy g_printer gadget */

static int major, minors;
static struct class *usb_gadget_class;
static DEFINE_IDA(printer_ida);
static DEFINE_MUTEX(printer_ida_lock); /* protects access do printer_ida */

/*-------------------------------------------------------------------------*/

struct printer_dev {
spinlock_t lock; /* lock this structure */
/* lock buffer lists during read/write calls */
struct mutex lock_printer_io;
struct usb_gadget *gadget;
s8 interface;
struct usb_ep *in_ep, *out_ep;
struct kref kref;
struct list_head rx_reqs; /* List of free RX structs */
struct list_head rx_reqs_active; /* List of Active RX xfers */
struct list_head rx_buffers; /* List of completed xfers */
/* wait until there is data to be read. */
wait_queue_head_t rx_wait;
struct list_head tx_reqs; /* List of free TX structs */
struct list_head tx_reqs_active; /* List of Active TX xfers */
/* Wait until there are write buffers available to use. */
wait_queue_head_t tx_wait;
/* Wait until all write buffers have been sent. */
wait_queue_head_t tx_flush_wait;
struct usb_request *current_rx_req;
size_t current_rx_bytes;
u8 *current_rx_buf;
u8 printer_status;
u8 reset_printer;
int minor;
struct cdev printer_cdev;
u8 printer_cdev_open;
wait_queue_head_t wait;
unsigned q_len;
char *pnp_string; /* We don't own memory! */
struct usb_function function;
};

static inline struct printer_dev *func_to_printer(struct usb_function *f)
{
return container_of(f, struct printer_dev, function);
}
/*-------------------------------------------------------------------------*/

/*
* DESCRIPTORS ... most are static, but strings and (full) configuration
* descriptors are built on demand.
*/

/* holds our biggest descriptor */
#define USB_DESC_BUFSIZE 256
#define USB_BUFSIZE 8192

static struct usb_interface_descriptor intf_desc = {
.bLength = sizeof(intf_desc),
.bDescriptorType = USB_DT_INTERFACE,
.bNumEndpoints = 4,
.bInterfaceClass = USB_CLASS_PER_INTERFACE,
.bInterfaceSubClass = USB_CLASS_PER_INTERFACE, /* Printer Sub-Class */
.bInterfaceProtocol = USB_CLASS_PER_INTERFACE, /* Bi-Directional */
.iInterface = 0
};

static struct usb_endpoint_descriptor fs_ep_in_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bEndpointAddress = USB_DIR_IN,
.bmAttributes = USB_ENDPOINT_XFER_BULK
};

static struct usb_endpoint_descriptor fs_ep_out_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bEndpointAddress = USB_DIR_OUT,
.bmAttributes = USB_ENDPOINT_XFER_BULK
};

static struct usb_endpoint_descriptor fs_ep1_in_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_IN | 0x02
};

static struct usb_endpoint_descriptor fs_ep1_out_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_OUT | 0x02
};

static struct usb_descriptor_header *fs_printer_function[] = {
(struct usb_descriptor_header *) &intf_desc,
(struct usb_descriptor_header *) &fs_ep_in_desc,
(struct usb_descriptor_header *) &fs_ep_out_desc,
(struct usb_descriptor_header *) &fs_ep1_in_desc,
(struct usb_descriptor_header *) &fs_ep1_out_desc,
NULL
};

/*
* usb 2.0 devices need to expose both high speed and full speed
* descriptors, unless they only run at full speed.
*/

static struct usb_endpoint_descriptor hs_ep_in_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_IN,
.wMaxPacketSize = cpu_to_le16(512)
};
//Commeted this to just get he ep1_out
static struct usb_endpoint_descriptor hs_ep_out_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_OUT,
.wMaxPacketSize = cpu_to_le16(512)
};
static struct usb_endpoint_descriptor hs_ep1_in_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_IN | 0x02,
.wMaxPacketSize = cpu_to_le16(512)
};

static struct usb_endpoint_descriptor hs_ep1_out_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_OUT | 0x02,
.wMaxPacketSize = cpu_to_le16(512)
};

static struct usb_descriptor_header *hs_printer_function[] = {
(struct usb_descriptor_header *) &intf_desc,
(struct usb_descriptor_header *) &hs_ep_in_desc,
(struct usb_descriptor_header *) &hs_ep_out_desc,
(struct usb_descriptor_header *) &hs_ep1_in_desc,
(struct usb_descriptor_header *) &hs_ep1_out_desc,
NULL
};

/*
* Added endpoint descriptors for 3.0 devices
*/

static struct usb_endpoint_descriptor ss_ep_in_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.wMaxPacketSize = cpu_to_le16(1024),
};

static struct usb_ss_ep_comp_descriptor ss_ep_in_comp_desc = {
.bLength = sizeof(ss_ep_in_comp_desc),
.bDescriptorType = USB_DT_SS_ENDPOINT_COMP,
};


static struct usb_endpoint_descriptor ss_ep_out_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.wMaxPacketSize = cpu_to_le16(1024),
};

static struct usb_ss_ep_comp_descriptor ss_ep_out_comp_desc = {
.bLength = sizeof(ss_ep_out_comp_desc),
.bDescriptorType = USB_DT_SS_ENDPOINT_COMP,
};

static struct usb_endpoint_descriptor ss_ep1_in_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_IN | 0x02,
.wMaxPacketSize = cpu_to_le16(1024)
};

static struct usb_ss_ep_comp_descriptor ss_ep1_in_comp_desc = {
.bLength = sizeof(ss_ep1_in_comp_desc),
.bDescriptorType = USB_DT_SS_ENDPOINT_COMP,
};


static struct usb_endpoint_descriptor ss_ep1_out_desc = {
.bLength = USB_DT_ENDPOINT_SIZE,
.bDescriptorType = USB_DT_ENDPOINT,
.bmAttributes = USB_ENDPOINT_XFER_BULK,
.bEndpointAddress = USB_DIR_OUT | 0x02,
.wMaxPacketSize = cpu_to_le16(1024)
};

static struct usb_ss_ep_comp_descriptor ss_ep1_out_comp_desc = {
.bLength = sizeof(ss_ep1_out_comp_desc),
.bDescriptorType = USB_DT_SS_ENDPOINT_COMP,
};

static struct usb_descriptor_header *ss_printer_function[] = {
(struct usb_descriptor_header *) &intf_desc,
(struct usb_descriptor_header *) &ss_ep_in_desc,
(struct usb_descriptor_header *) &ss_ep_in_comp_desc,
(struct usb_descriptor_header *) &ss_ep_out_desc,
(struct usb_descriptor_header *) &ss_ep_out_comp_desc,
(struct usb_descriptor_header *) &ss_ep1_in_desc,
(struct usb_descriptor_header *) &ss_ep1_in_comp_desc,
(struct usb_descriptor_header *) &ss_ep1_out_desc,
(struct usb_descriptor_header *) &ss_ep1_out_comp_desc,
NULL
};

/* maxpacket and other transfer characteristics vary by speed. */
static inline struct usb_endpoint_descriptor *ep_desc(struct usb_gadget *gadget,
struct usb_endpoint_descriptor *fs,
struct usb_endpoint_descriptor *hs,
struct usb_endpoint_descriptor *ss)
{
switch (gadget->speed) {
case USB_SPEED_SUPER:
return ss;
case USB_SPEED_HIGH:
return hs;
default:
return fs;
}
}

/*-------------------------------------------------------------------------*/

static void printer_dev_free(struct kref *kref)
{
struct printer_dev *dev = container_of(kref, struct printer_dev, kref);

kfree(dev);
}

static struct usb_request *
printer_req_alloc(struct usb_ep *ep, unsigned len, gfp_t gfp_flags)
{
struct usb_request *req;

req = usb_ep_alloc_request(ep, gfp_flags);

if (req != NULL) {
req->length = len;
req->buf = kmalloc(len, gfp_flags);
if (req->buf == NULL) {
usb_ep_free_request(ep, req);
return NULL;
}
}

return req;
}

static void
printer_req_free(struct usb_ep *ep, struct usb_request *req)
{
if (ep != NULL && req != NULL) {
kfree(req->buf);
usb_ep_free_request(ep, req);
}
}

/*-------------------------------------------------------------------------*/

static void rx_complete(struct usb_ep *ep, struct usb_request *req)
{
struct printer_dev *dev = ep->driver_data;
int status = req->status;
unsigned long flags;

spin_lock_irqsave(&dev->lock, flags);

list_del_init(&req->list); /* Remode from Active List */

switch (status) {

/* normal completion */
case 0:
if (req->actual > 0) {
list_add_tail(&req->list, &dev->rx_buffers);
DBG(dev, "G_Printer : rx length %d\n", req->actual);
} else {
list_add(&req->list, &dev->rx_reqs);
}
break;

/* software-driven interface shutdown */
case -ECONNRESET: /* unlink */
case -ESHUTDOWN: /* disconnect etc */
VDBG(dev, "rx shutdown, code %d\n", status);
list_add(&req->list, &dev->rx_reqs);
break;

/* for hardware automagic (such as pxa) */
case -ECONNABORTED: /* endpoint reset */
DBG(dev, "rx %s reset\n", ep->name);
list_add(&req->list, &dev->rx_reqs);
break;

/* data overrun */
case -EOVERFLOW:
fallthrough;

default:
DBG(dev, "rx status %d\n", status);
list_add(&req->list, &dev->rx_reqs);
break;
}

wake_up_interruptible(&dev->rx_wait);
spin_unlock_irqrestore(&dev->lock, flags);
}

static void tx_complete(struct usb_ep *ep, struct usb_request *req)
{
struct printer_dev *dev = ep->driver_data;

switch (req->status) {
default:
VDBG(dev, "tx err %d\n", req->status);
fallthrough;
case -ECONNRESET: /* unlink */
case -ESHUTDOWN: /* disconnect etc */
break;
case 0:
break;
}

spin_lock(&dev->lock);
/* Take the request struct off the active list and put it on the
* free list.
*/
list_del_init(&req->list);
list_add(&req->list, &dev->tx_reqs);
wake_up_interruptible(&dev->tx_wait);
if (likely(list_empty(&dev->tx_reqs_active)))
wake_up_interruptible(&dev->tx_flush_wait);

spin_unlock(&dev->lock);
}

/*-------------------------------------------------------------------------*/

static int
printer_open(struct inode *inode, struct file *fd)
{
struct printer_dev *dev;
unsigned long flags;
int ret = -EBUSY;

dev = container_of(inode->i_cdev, struct printer_dev, printer_cdev);

spin_lock_irqsave(&dev->lock, flags);

if (dev->interface < 0) {
spin_unlock_irqrestore(&dev->lock, flags);
return -ENODEV;
}
printk(KERN_INFO "Opening Sonosa Driver=================\n");
if (!dev->printer_cdev_open) {
dev->printer_cdev_open = 1;
fd->private_data = dev;
ret = 0;
/* Change the printer status to show that it's on-line. */
dev->printer_status |= PRINTER_SELECTED;
}

spin_unlock_irqrestore(&dev->lock, flags);

kref_get(&dev->kref);
DBG(dev, "Sonosa_open returned %x\n", ret);
return ret;
}

static int
printer_close(struct inode *inode, struct file *fd)
{
struct printer_dev *dev = fd->private_data;
unsigned long flags;

spin_lock_irqsave(&dev->lock, flags);
dev->printer_cdev_open = 0;
fd->private_data = NULL;
/* Change printer status to show that the printer is off-line. */
dev->printer_status &= ~PRINTER_SELECTED;
spin_unlock_irqrestore(&dev->lock, flags);

kref_put(&dev->kref, printer_dev_free);
DBG(dev, "Sonosa_close\n");

return 0;
}

/* This function must be called with interrupts turned off. */
static void
setup_rx_reqs(struct printer_dev *dev)
{
struct usb_request *req;

while (likely(!list_empty(&dev->rx_reqs))) {
int error;

req = container_of(dev->rx_reqs.next,
struct usb_request, list);
list_del_init(&req->list);

/* The USB Host sends us whatever amount of data it wants to
* so we always set the length field to the full USB_BUFSIZE.
* If the amount of data is more than the read() caller asked
* for it will be stored in the request buffer until it is
* asked for by read().
*/
req->length = USB_BUFSIZE;
req->complete = rx_complete;

/* here, we unlock, and only unlock, to avoid deadlock. */
spin_unlock(&dev->lock);
error = usb_ep_queue(dev->out_ep, req, GFP_ATOMIC);
spin_lock(&dev->lock);
if (error) {
DBG(dev, "rx submit --> %d\n", error);
list_add(&req->list, &dev->rx_reqs);
break;
}
/* if the req is empty, then add it into dev->rx_reqs_active. */
else if (list_empty(&req->list))
list_add(&req->list, &dev->rx_reqs_active);
}
}

static ssize_t
printer_read(struct file *fd, char __user *buf, size_t len, loff_t *ptr)
{
struct printer_dev *dev = fd->private_data;
unsigned long flags;
size_t size;
size_t bytes_copied;
struct usb_request *req;
/* This is a pointer to the current USB rx request. */
struct usb_request *current_rx_req;
/* This is the number of bytes in the current rx buffer. */
size_t current_rx_bytes;
/* This is a pointer to the current rx buffer. */
u8 *current_rx_buf;

if (len == 0)
return -EINVAL;

DBG(dev, "sonosa_read trying to read %d bytes\n", (int)len);
printk(KERN_INFO "Sonosa Read=================:\n");
mutex_lock(&dev->lock_printer_io);
spin_lock_irqsave(&dev->lock, flags);

if (dev->interface < 0) {
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);
return -ENODEV;
}

/* We will use this flag later to check if a printer reset happened
* after we turn interrupts back on.
*/
dev->reset_printer = 0;

setup_rx_reqs(dev);

bytes_copied = 0;
current_rx_req = dev->current_rx_req;
current_rx_bytes = dev->current_rx_bytes;
current_rx_buf = dev->current_rx_buf;
dev->current_rx_req = NULL;
dev->current_rx_bytes = 0;
dev->current_rx_buf = NULL;

/* Check if there is any data in the read buffers. Please note that
* current_rx_bytes is the number of bytes in the current rx buffer.
* If it is zero then check if there are any other rx_buffers that
* are on the completed list. We are only out of data if all rx
* buffers are empty.
*/
if ((current_rx_bytes == 0) &&
(likely(list_empty(&dev->rx_buffers)))) {
/* Turn interrupts back on before sleeping. */
spin_unlock_irqrestore(&dev->lock, flags);

/*
* If no data is available check if this is a NON-Blocking
* call or not.
*/
if (fd->f_flags & (O_NONBLOCK|O_NDELAY)) {
mutex_unlock(&dev->lock_printer_io);
return -EAGAIN;
}

/* Sleep until data is available */
wait_event_interruptible(dev->rx_wait,
(likely(!list_empty(&dev->rx_buffers))));
spin_lock_irqsave(&dev->lock, flags);
}

/* We have data to return then copy it to the caller's buffer.*/
while ((current_rx_bytes || likely(!list_empty(&dev->rx_buffers)))
&& len) {
if (current_rx_bytes == 0) {
req = container_of(dev->rx_buffers.next,
struct usb_request, list);
list_del_init(&req->list);

if (req->actual && req->buf) {
current_rx_req = req;
current_rx_bytes = req->actual;
current_rx_buf = req->buf;
} else {
list_add(&req->list, &dev->rx_reqs);
continue;
}
}

/* Don't leave irqs off while doing memory copies */
spin_unlock_irqrestore(&dev->lock, flags);

if (len > current_rx_bytes)
size = current_rx_bytes;
else
size = len;

size -= copy_to_user(buf, current_rx_buf, size);
bytes_copied += size;
len -= size;
buf += size;

spin_lock_irqsave(&dev->lock, flags);

/* We've disconnected or reset so return. */
if (dev->reset_printer) {
list_add(&current_rx_req->list, &dev->rx_reqs);
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);
return -EAGAIN;
}

/* If we not returning all the data left in this RX request
* buffer then adjust the amount of data left in the buffer.
* Othewise if we are done with this RX request buffer then
* requeue it to get any incoming data from the USB host.
*/
if (size < current_rx_bytes) {
current_rx_bytes -= size;
current_rx_buf += size;
} else {
list_add(&current_rx_req->list, &dev->rx_reqs);
current_rx_bytes = 0;
current_rx_buf = NULL;
current_rx_req = NULL;
}
}

dev->current_rx_req = current_rx_req;
dev->current_rx_bytes = current_rx_bytes;
dev->current_rx_buf = current_rx_buf;

spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);

DBG(dev, "printer_read returned %d bytes\n", (int)bytes_copied);

if (bytes_copied)
return bytes_copied;
else
return -EAGAIN;
}

static ssize_t
printer_write(struct file *fd, const char __user *buf, size_t len, loff_t *ptr)
{
struct printer_dev *dev = fd->private_data;
unsigned long flags;
size_t size; /* Amount of data in a TX request. */
size_t bytes_copied = 0;
struct usb_request *req;
int value;

DBG(dev, "printer_write trying to send %d bytes\n", (int)len);

if (len == 0)
return -EINVAL;

mutex_lock(&dev->lock_printer_io);
spin_lock_irqsave(&dev->lock, flags);

if (dev->interface < 0) {
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);
return -ENODEV;
}

/* Check if a printer reset happens while we have interrupts on */
dev->reset_printer = 0;

/* Check if there is any available write buffers */
if (likely(list_empty(&dev->tx_reqs))) {
/* Turn interrupts back on before sleeping. */
spin_unlock_irqrestore(&dev->lock, flags);

/*
* If write buffers are available check if this is
* a NON-Blocking call or not.
*/
if (fd->f_flags & (O_NONBLOCK|O_NDELAY)) {
mutex_unlock(&dev->lock_printer_io);
return -EAGAIN;
}

/* Sleep until a write buffer is available */
wait_event_interruptible(dev->tx_wait,
(likely(!list_empty(&dev->tx_reqs))));
spin_lock_irqsave(&dev->lock, flags);
}

while (likely(!list_empty(&dev->tx_reqs)) && len) {

if (len > USB_BUFSIZE)
size = USB_BUFSIZE;
else
size = len;

req = container_of(dev->tx_reqs.next, struct usb_request,
list);
list_del_init(&req->list);

req->complete = tx_complete;
req->length = size;

/* Check if we need to send a zero length packet. */
if (len > size)
/* They will be more TX requests so no yet. */
req->zero = 0;
else
/* If the data amount is not a multiple of the
* maxpacket size then send a zero length packet.
*/
req->zero = ((len % dev->in_ep->maxpacket) == 0);

/* Don't leave irqs off while doing memory copies */
spin_unlock_irqrestore(&dev->lock, flags);

if (copy_from_user(req->buf, buf, size)) {
list_add(&req->list, &dev->tx_reqs);
mutex_unlock(&dev->lock_printer_io);
return bytes_copied;
}

bytes_copied += size;
len -= size;
buf += size;

spin_lock_irqsave(&dev->lock, flags);

/* We've disconnected or reset so free the req and buffer */
if (dev->reset_printer) {
list_add(&req->list, &dev->tx_reqs);
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);
return -EAGAIN;
}

list_add(&req->list, &dev->tx_reqs_active);

/* here, we unlock, and only unlock, to avoid deadlock. */
spin_unlock(&dev->lock);
value = usb_ep_queue(dev->in_ep, req, GFP_ATOMIC);
spin_lock(&dev->lock);
if (value) {
list_move(&req->list, &dev->tx_reqs);
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);
return -EAGAIN;
}
}

spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);

DBG(dev, "printer_write sent %d bytes\n", (int)bytes_copied);

if (bytes_copied)
return bytes_copied;
else
return -EAGAIN;
}

static int
printer_fsync(struct file *fd, loff_t start, loff_t end, int datasync)
{
struct printer_dev *dev = fd->private_data;
struct inode *inode = file_inode(fd);
unsigned long flags;
int tx_list_empty;

inode_lock(inode);
spin_lock_irqsave(&dev->lock, flags);

if (dev->interface < 0) {
spin_unlock_irqrestore(&dev->lock, flags);
inode_unlock(inode);
return -ENODEV;
}

tx_list_empty = (likely(list_empty(&dev->tx_reqs)));
spin_unlock_irqrestore(&dev->lock, flags);

if (!tx_list_empty) {
/* Sleep until all data has been sent */
wait_event_interruptible(dev->tx_flush_wait,
(likely(list_empty(&dev->tx_reqs_active))));
}
inode_unlock(inode);

return 0;
}

static __poll_t
printer_poll(struct file *fd, poll_table *wait)
{
struct printer_dev *dev = fd->private_data;
unsigned long flags;
__poll_t status = 0;

mutex_lock(&dev->lock_printer_io);
spin_lock_irqsave(&dev->lock, flags);

if (dev->interface < 0) {
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);
return EPOLLERR | EPOLLHUP;
}

setup_rx_reqs(dev);
spin_unlock_irqrestore(&dev->lock, flags);
mutex_unlock(&dev->lock_printer_io);

poll_wait(fd, &dev->rx_wait, wait);
poll_wait(fd, &dev->tx_wait, wait);

spin_lock_irqsave(&dev->lock, flags);
if (likely(!list_empty(&dev->tx_reqs)))
status |= EPOLLOUT | EPOLLWRNORM;

if (likely(dev->current_rx_bytes) ||
likely(!list_empty(&dev->rx_buffers)))
status |= EPOLLIN | EPOLLRDNORM;

spin_unlock_irqrestore(&dev->lock, flags);

return status;
}

static long
printer_ioctl(struct file *fd, unsigned int code, unsigned long arg)
{
struct printer_dev *dev = fd->private_data;
unsigned long flags;
int status = 0;

DBG(dev, "printer_ioctl: cmd=0x%4.4x, arg=%lu\n", code, arg);

/* handle ioctls */

spin_lock_irqsave(&dev->lock, flags);

if (dev->interface < 0) {
spin_unlock_irqrestore(&dev->lock, flags);
return -ENODEV;
}

switch (code) {
case GADGET_GET_PRINTER_STATUS:
status = (int)dev->printer_status;
break;
case GADGET_SET_PRINTER_STATUS:
dev->printer_status = (u8)arg;
break;
default:
/* could not handle ioctl */
DBG(dev, "printer_ioctl: ERROR cmd=0x%4.4xis not supported\n",
code);
status = -ENOTTY;
}

spin_unlock_irqrestore(&dev->lock, flags);

return status;
}

/* used after endpoint configuration */
static const struct file_operations printer_io_operations = {
.owner = THIS_MODULE,
.open = printer_open,
.read = printer_read,
.write = printer_write,
.fsync = printer_fsync,
.poll = printer_poll,
.unlocked_ioctl = printer_ioctl,
.release = printer_close,
.llseek = noop_llseek,
};

/*-------------------------------------------------------------------------*/

static int
set_printer_interface(struct printer_dev *dev)
{
int result = 0;

dev->in_ep->desc = ep_desc(dev->gadget, &fs_ep_in_desc, &hs_ep_in_desc,
&ss_ep_in_desc);
dev->in_ep->driver_data = dev;

dev->out_ep->desc = ep_desc(dev->gadget, &fs_ep_out_desc,
&hs_ep1_out_desc,&ss_ep_out_desc);
dev->out_ep->driver_data = dev;

result = usb_ep_enable(dev->in_ep);
if (result != 0) {
DBG(dev, "enable %s --> %d\n", dev->in_ep->name, result);
printk(KERN_INFO, "Enabling Endpoints+++++++++++++++++++");
goto done;
}

result = usb_ep_enable(dev->out_ep);
if (result != 0) {
DBG(dev, "enable %s --> %d\n", dev->out_ep->name, result);
goto done;
}

done:
/* on error, disable any endpoints */
if (result != 0) {
(void) usb_ep_disable(dev->in_ep);
(void) usb_ep_disable(dev->out_ep);
dev->in_ep->desc = NULL;
dev->out_ep->desc = NULL;
}

/* caller is responsible for cleanup on error */
return result;
}

static void printer_reset_interface(struct printer_dev *dev)
{
unsigned long flags;

if (dev->interface < 0)
return;

DBG(dev, "%s\n", __func__);

if (dev->in_ep->desc)
usb_ep_disable(dev->in_ep);

if (dev->out_ep->desc)
usb_ep_disable(dev->out_ep);

spin_lock_irqsave(&dev->lock, flags);
dev->in_ep->desc = NULL;
dev->out_ep->desc = NULL;
dev->interface = -1;
spin_unlock_irqrestore(&dev->lock, flags);
}

/* Change our operational Interface. */
static int set_interface(struct printer_dev *dev, unsigned number)
{
int result = 0;

/* Free the current interface */
printer_reset_interface(dev);

result = set_printer_interface(dev);
if (result)
printer_reset_interface(dev);
else
dev->interface = number;

if (!result)
INFO(dev, "Using interface %x\n", number);

return result;
}

static void printer_soft_reset(struct printer_dev *dev)
{
struct usb_request *req;

INFO(dev, "Received Printer Reset Request\n");

if (usb_ep_disable(dev->in_ep))
DBG(dev, "Failed to disable USB in_ep\n");
if (usb_ep_disable(dev->out_ep))
DBG(dev, "Failed to disable USB out_ep\n");

if (dev->current_rx_req != NULL) {
list_add(&dev->current_rx_req->list, &dev->rx_reqs);
dev->current_rx_req = NULL;
}
dev->current_rx_bytes = 0;
dev->current_rx_buf = NULL;
dev->reset_printer = 1;

while (likely(!(list_empty(&dev->rx_buffers)))) {
req = container_of(dev->rx_buffers.next, struct usb_request,
list);
list_del_init(&req->list);
list_add(&req->list, &dev->rx_reqs);
}

while (likely(!(list_empty(&dev->rx_reqs_active)))) {
req = container_of(dev->rx_buffers.next, struct usb_request,
list);
list_del_init(&req->list);
list_add(&req->list, &dev->rx_reqs);
}

while (likely(!(list_empty(&dev->tx_reqs_active)))) {
req = container_of(dev->tx_reqs_active.next,
struct usb_request, list);
list_del_init(&req->list);
list_add(&req->list, &dev->tx_reqs);
}

if (usb_ep_enable(dev->in_ep))
DBG(dev, "Failed to enable USB in_ep\n");
if (usb_ep_enable(dev->out_ep))
DBG(dev, "Failed to enable USB out_ep\n");

wake_up_interruptible(&dev->rx_wait);
wake_up_interruptible(&dev->tx_wait);
wake_up_interruptible(&dev->tx_flush_wait);
}

/*-------------------------------------------------------------------------*/

static bool gprinter_req_match(struct usb_function *f,
const struct usb_ctrlrequest *ctrl,
bool config0)
{
struct printer_dev *dev = func_to_printer(f);
u16 w_index = le16_to_cpu(ctrl->wIndex);
u16 w_value = le16_to_cpu(ctrl->wValue);
u16 w_length = le16_to_cpu(ctrl->wLength);

if (config0)
return false;

if ((ctrl->bRequestType & USB_RECIP_MASK) != USB_RECIP_INTERFACE ||
(ctrl->bRequestType & USB_TYPE_MASK) != USB_TYPE_CLASS)
return false;

switch (ctrl->bRequest) {
case GET_DEVICE_ID:
w_index >>= 8;
if (USB_DIR_IN & ctrl->bRequestType)
break;
return false;
case GET_PORT_STATUS:
if (!w_value && w_length == 1 &&
(USB_DIR_IN & ctrl->bRequestType))
break;
return false;
case SOFT_RESET:
if (!w_value && !w_length &&
!(USB_DIR_IN & ctrl->bRequestType))
break;
fallthrough;
default:
return false;
}
return w_index == dev->interface;
}

/*
* The setup() callback implements all the ep0 functionality that's not
* handled lower down.
*/
static int printer_func_setup(struct usb_function *f,
const struct usb_ctrlrequest *ctrl)
{
struct printer_dev *dev = func_to_printer(f);
struct usb_composite_dev *cdev = f->config->cdev;
struct usb_request *req = cdev->req;
u8 *buf = req->buf;
int value = -EOPNOTSUPP;
u16 wIndex = le16_to_cpu(ctrl->wIndex);
u16 wValue = le16_to_cpu(ctrl->wValue);
u16 wLength = le16_to_cpu(ctrl->wLength);

DBG(dev, "ctrl req%02x.%02x v%04x i%04x l%d\n",
ctrl->bRequestType, ctrl->bRequest, wValue, wIndex, wLength);

switch (ctrl->bRequestType&USB_TYPE_MASK) {
case USB_TYPE_CLASS:
switch (ctrl->bRequest) {
case GET_DEVICE_ID: /* Get the IEEE-1284 PNP String */
/* Only one printer interface is supported. */
if ((wIndex>>8) != dev->interface)
break;

if (!dev->pnp_string) {
value = 0;
break;
}
value = strlen(dev->pnp_string);
buf[0] = (value >> & 0xFF;
buf[1] = value & 0xFF;
memcpy(buf + 2, dev->pnp_string, value);
DBG(dev, "1284 PNP String: %x %s\n", value,
dev->pnp_string);
break;

case GET_PORT_STATUS: /* Get Port Status */
/* Only one printer interface is supported. */
if (wIndex != dev->interface)
break;

buf[0] = dev->printer_status;
value = min_t(u16, wLength, 1);
break;

case SOFT_RESET: /* Soft Reset */
/* Only one printer interface is supported. */
if (wIndex != dev->interface)
break;

printer_soft_reset(dev);

value = 0;
break;

default:
goto unknown;
}
break;

default:
unknown:
VDBG(dev,
"unknown ctrl req%02x.%02x v%04x i%04x l%d\n",
ctrl->bRequestType, ctrl->bRequest,
wValue, wIndex, wLength);
break;
}
/* host either stalls (value < 0) or reports success */
if (value >= 0) {
req->length = value;
req->zero = value < wLength;
value = usb_ep_queue(cdev->gadget->ep0, req, GFP_ATOMIC);
if (value < 0) {
ERROR(dev, "%s:%d Error!\n", __func__, __LINE__);
req->status = 0;
}
}
return value;
}

static int printer_func_bind(struct usb_configuration *c,
struct usb_function *f)
{
struct usb_gadget *gadget = c->cdev->gadget;
struct printer_dev *dev = func_to_printer(f);
struct device *pdev;
struct usb_composite_dev *cdev = c->cdev;
struct usb_ep *in_ep;
struct usb_ep *out_ep = NULL;
struct usb_request *req;
int id;
int ret;
u32 i;
dev_t devt;
id = usb_interface_id(c, f);
if (id < 0)
return id;
intf_desc.bInterfaceNumber = id;

/* finish hookup to lower layer ... */
dev->gadget = gadget;

/* all we really need is bulk IN/OUT */
in_ep = usb_ep_autoconfig(cdev->gadget, &fs_ep_in_desc);
if (!in_ep) {
autoconf_fail:
dev_err(&cdev->gadget->dev, "can't autoconfigure on %s\n",
cdev->gadget->name);
return -ENODEV;
}

out_ep = usb_ep_autoconfig(cdev->gadget, &fs_ep_out_desc);
if (!out_ep)
goto autoconf_fail;

/* assumes that all endpoints are dual-speed */
hs_ep_in_desc.bEndpointAddress = fs_ep_in_desc.bEndpointAddress;
// hs_ep_out_desc.bEndpointAddress = fs_ep_out_desc.bEndpointAddress;
hs_ep1_out_desc.bEndpointAddress = fs_ep_in_desc.bEndpointAddress;
// hs_ep1_out_desc.bEndpointAddress = fs_ep_out_desc.bEndpointAddress;
ss_ep_in_desc.bEndpointAddress = fs_ep_in_desc.bEndpointAddress;
ss_ep_out_desc.bEndpointAddress = fs_ep_out_desc.bEndpointAddress;

ret = usb_assign_descriptors(f, fs_printer_function,
hs_printer_function, ss_printer_function,
ss_printer_function);
if (ret)
return ret;

dev->in_ep = in_ep;
dev->out_ep = out_ep;

ret = -ENOMEM;
for (i = 0; i < dev->q_len; i++) {
req = printer_req_alloc(dev->in_ep, USB_BUFSIZE, GFP_KERNEL);
if (!req)
goto fail_tx_reqs;
list_add(&req->list, &dev->tx_reqs);
}

for (i = 0; i < dev->q_len; i++) {
req = printer_req_alloc(dev->out_ep, USB_BUFSIZE, GFP_KERNEL);
if (!req)
goto fail_rx_reqs;
list_add(&req->list, &dev->rx_reqs);
}

/* Setup the sysfs files for the printer gadget. */
devt = MKDEV(major, dev->minor);
pdev = device_create(usb_gadget_class, NULL, devt,
NULL, "sonosa_acu%d", dev->minor);
if (IS_ERR(pdev)) {
ERROR(dev, "Failed to create device: sonosa_acu\n");
ret = PTR_ERR(pdev);
goto fail_rx_reqs;
}

/*
* Register a character device as an interface to a user mode
* program that handles the printer specific functionality.
*/
cdev_init(&dev->printer_cdev, &printer_io_operations);
dev->printer_cdev.owner = THIS_MODULE;
ret = cdev_add(&dev->printer_cdev, devt, 1);
if (ret) {
ERROR(dev, "Failed to open char device\n");
goto fail_cdev_add;
}

return 0;

fail_cdev_add:
device_destroy(usb_gadget_class, devt);

fail_rx_reqs:
while (!list_empty(&dev->rx_reqs)) {
req = container_of(dev->rx_reqs.next, struct usb_request, list);
list_del(&req->list);
printer_req_free(dev->out_ep, req);
}

fail_tx_reqs:
while (!list_empty(&dev->tx_reqs)) {
req = container_of(dev->tx_reqs.next, struct usb_request, list);
list_del(&req->list);
printer_req_free(dev->in_ep, req);
}

usb_free_all_descriptors(f);
return ret;

}

static int printer_func_set_alt(struct usb_function *f,
unsigned intf, unsigned alt)
{
struct printer_dev *dev = func_to_printer(f);
int ret = -ENOTSUPP;

if (!alt)
ret = set_interface(dev, intf);

return ret;
}

static void printer_func_disable(struct usb_function *f)
{
struct printer_dev *dev = func_to_printer(f);

DBG(dev, "%s\n", __func__);

printer_reset_interface(dev);
}

static inline struct f_printer_opts
*to_f_printer_opts(struct config_item *item)
{
return container_of(to_config_group(item), struct f_printer_opts,
func_inst.group);
}

static void printer_attr_release(struct config_item *item)
{
struct f_printer_opts *opts = to_f_printer_opts(item);

usb_put_function_instance(&opts->func_inst);
}

static struct configfs_item_operations printer_item_ops = {
.release = printer_attr_release,
};

static ssize_t f_printer_opts_pnp_string_show(struct config_item *item,
char *page)
{
struct f_printer_opts *opts = to_f_printer_opts(item);
int result = 0;

mutex_lock(&opts->lock);
if (!opts->pnp_string)
goto unlock;

result = strlcpy(page, opts->pnp_string, PAGE_SIZE);
if (result >= PAGE_SIZE) {
result = PAGE_SIZE;
} else if (page[result - 1] != '\n' && result + 1 < PAGE_SIZE) {
page[result++] = '\n';
page[result] = '\0';
}

unlock:
mutex_unlock(&opts->lock);

return result;
}

static ssize_t f_printer_opts_pnp_string_store(struct config_item *item,
const char *page, size_t len)
{
struct f_printer_opts *opts = to_f_printer_opts(item);
char *new_pnp;
int result;

mutex_lock(&opts->lock);

new_pnp = kstrndup(page, len, GFP_KERNEL);
if (!new_pnp) {
result = -ENOMEM;
goto unlock;
}

if (opts->pnp_string_allocated)
kfree(opts->pnp_string);

opts->pnp_string_allocated = true;
opts->pnp_string = new_pnp;
result = len;
unlock:
mutex_unlock(&opts->lock);

return result;
}

CONFIGFS_ATTR(f_printer_opts_, pnp_string);

static ssize_t f_printer_opts_q_len_show(struct config_item *item,
char *page)
{
struct f_printer_opts *opts = to_f_printer_opts(item);
int result;

mutex_lock(&opts->lock);
result = sprintf(page, "%d\n", opts->q_len);
mutex_unlock(&opts->lock);

return result;
}

static ssize_t f_printer_opts_q_len_store(struct config_item *item,
const char *page, size_t len)
{
struct f_printer_opts *opts = to_f_printer_opts(item);
int ret;
u16 num;

mutex_lock(&opts->lock);
if (opts->refcnt) {
ret = -EBUSY;
goto end;
}

ret = kstrtou16(page, 0, &num);
if (ret)
goto end;

opts->q_len = (unsigned)num;
ret = len;
end:
mutex_unlock(&opts->lock);
return ret;
}

CONFIGFS_ATTR(f_printer_opts_, q_len);

static struct configfs_attribute *printer_attrs[] = {
&f_printer_opts_attr_pnp_string,
&f_printer_opts_attr_q_len,
NULL,
};

static const struct config_item_type printer_func_type = {
.ct_item_ops = &printer_item_ops,
.ct_attrs = printer_attrs,
.ct_owner = THIS_MODULE,
};

static inline int gprinter_get_minor(void)
{
int ret;

ret = ida_simple_get(&printer_ida, 0, 0, GFP_KERNEL);
if (ret >= PRINTER_MINORS) {
ida_simple_remove(&printer_ida, ret);
ret = -ENODEV;
}

return ret;
}

static inline void gprinter_put_minor(int minor)
{
ida_simple_remove(&printer_ida, minor);
}

static int gprinter_setup(int);
static void gprinter_cleanup(void);

static void gprinter_free_inst(struct usb_function_instance *f)
{
struct f_printer_opts *opts;

opts = container_of(f, struct f_printer_opts, func_inst);

mutex_lock(&printer_ida_lock);

gprinter_put_minor(opts->minor);
if (ida_is_empty(&printer_ida))
gprinter_cleanup();

mutex_unlock(&printer_ida_lock);

if (opts->pnp_string_allocated)
kfree(opts->pnp_string);
kfree(opts);
}

static struct usb_function_instance *gprinter_alloc_inst(void)
{
struct f_printer_opts *opts;
struct usb_function_instance *ret;
int status = 0;

opts = kzalloc(sizeof(*opts), GFP_KERNEL);
if (!opts)
return ERR_PTR(-ENOMEM);

mutex_init(&opts->lock);
opts->func_inst.free_func_inst = gprinter_free_inst;
ret = &opts->func_inst;

/* Make sure q_len is initialized, otherwise the bound device can't support read/write! */
opts->q_len = DEFAULT_Q_LEN;

mutex_lock(&printer_ida_lock);

if (ida_is_empty(&printer_ida)) {
status = gprinter_setup(PRINTER_MINORS);
if (status) {
ret = ERR_PTR(status);
kfree(opts);
goto unlock;
}
}

opts->minor = gprinter_get_minor();
if (opts->minor < 0) {
ret = ERR_PTR(opts->minor);
kfree(opts);
if (ida_is_empty(&printer_ida))
gprinter_cleanup();
goto unlock;
}
config_group_init_type_name(&opts->func_inst.group, "",
&printer_func_type);

unlock:
mutex_unlock(&printer_ida_lock);
return ret;
}

static void gprinter_free(struct usb_function *f)
{
struct printer_dev *dev = func_to_printer(f);
struct f_printer_opts *opts;

opts = container_of(f->fi, struct f_printer_opts, func_inst);

kref_put(&dev->kref, printer_dev_free);
mutex_lock(&opts->lock);
--opts->refcnt;
mutex_unlock(&opts->lock);
}

static void printer_func_unbind(struct usb_configuration *c,
struct usb_function *f)
{
struct printer_dev *dev;
struct usb_request *req;

dev = func_to_printer(f);

device_destroy(usb_gadget_class, MKDEV(major, dev->minor));

/* Remove Character Device */
cdev_del(&dev->printer_cdev);

/* we must already have been disconnected ... no i/o may be active */
WARN_ON(!list_empty(&dev->tx_reqs_active));
WARN_ON(!list_empty(&dev->rx_reqs_active));

/* Free all memory for this driver. */
while (!list_empty(&dev->tx_reqs)) {
req = container_of(dev->tx_reqs.next, struct usb_request,
list);
list_del(&req->list);
printer_req_free(dev->in_ep, req);
}

if (dev->current_rx_req != NULL)
printer_req_free(dev->out_ep, dev->current_rx_req);

while (!list_empty(&dev->rx_reqs)) {
req = container_of(dev->rx_reqs.next,
struct usb_request, list);
list_del(&req->list);
printer_req_free(dev->out_ep, req);
}

while (!list_empty(&dev->rx_buffers)) {
req = container_of(dev->rx_buffers.next,
struct usb_request, list);
list_del(&req->list);
printer_req_free(dev->out_ep, req);
}
usb_free_all_descriptors(f);
}

static struct usb_function *gprinter_alloc(struct usb_function_instance *fi)
{
struct printer_dev *dev;
struct f_printer_opts *opts;

opts = container_of(fi, struct f_printer_opts, func_inst);

mutex_lock(&opts->lock);
if (opts->minor >= minors) {
mutex_unlock(&opts->lock);
return ERR_PTR(-ENOENT);
}

dev = kzalloc(sizeof(*dev), GFP_KERNEL);
if (!dev) {
mutex_unlock(&opts->lock);
return ERR_PTR(-ENOMEM);
}

kref_init(&dev->kref);
++opts->refcnt;
dev->minor = opts->minor;
dev->pnp_string = opts->pnp_string;
dev->q_len = opts->q_len;
mutex_unlock(&opts->lock);

dev->function.name = "printer";
dev->function.bind = printer_func_bind;
dev->function.setup = printer_func_setup;
dev->function.unbind = printer_func_unbind;
dev->function.set_alt = printer_func_set_alt;
dev->function.disable = printer_func_disable;
dev->function.req_match = gprinter_req_match;
dev->function.free_func = gprinter_free;

INIT_LIST_HEAD(&dev->tx_reqs);
INIT_LIST_HEAD(&dev->rx_reqs);
INIT_LIST_HEAD(&dev->rx_buffers);
INIT_LIST_HEAD(&dev->tx_reqs_active);
INIT_LIST_HEAD(&dev->rx_reqs_active);

spin_lock_init(&dev->lock);
mutex_init(&dev->lock_printer_io);
init_waitqueue_head(&dev->rx_wait);
init_waitqueue_head(&dev->tx_wait);
init_waitqueue_head(&dev->tx_flush_wait);

dev->interface = -1;
dev->printer_cdev_open = 0;
dev->printer_status = PRINTER_NOT_ERROR;
dev->current_rx_req = NULL;
dev->current_rx_bytes = 0;
dev->current_rx_buf = NULL;

return &dev->function;
}

DECLARE_USB_FUNCTION_INIT(printer, gprinter_alloc_inst, gprinter_alloc);
MODULE_LICENSE("GPL");
MODULE_AUTHOR("Craig Nadler");

static int gprinter_setup(int count)
{
int status;
dev_t devt;

usb_gadget_class = class_create(THIS_MODULE, "usb_printer_gadget");
//usb_gadget_class = class_create(THIS_MODULE, "sonosa_acu");
if (IS_ERR(usb_gadget_class)) {
status = PTR_ERR(usb_gadget_class);
usb_gadget_class = NULL;
pr_err("unable to create usb_gadget class %d\n", status);
return status;
}
status = alloc_chrdev_region(&devt, 0, count, "sonosa_acu");
if (status) {
pr_err("alloc_chrdev_region %d\n", status);
class_destroy(usb_gadget_class);
usb_gadget_class = NULL;
return status;
}

major = MAJOR(devt);
minors = count;

return status;
}

static void gprinter_cleanup(void)
{
if (major) {
unregister_chrdev_region(MKDEV(major, 0), minors);
major = minors = 0;
}
class_destroy(usb_gadget_class);
usb_gadget_class= NULL;
}

0 件の賞賛
返信