UUU tools failed flashing U-boot into nand with custom logo on iMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UUU tools failed flashing U-boot into nand with custom logo on iMX6ULL

Jump to solution
1,369 Views
91_quyetluu
Contributor II

Hi All,
I want to custom logo in U-boot with my one. 

I converted my logo and tested successfully with bmp display command in U-boot. Now I want to hard the logo in booting with my custom one. I replaced freescale.bmp by my bmp file. I check the bmp_logo.h which is generated by tools in uboot and it seems correct (size, format). When I used UUU tool to flash this U-boot to Nand, I have problem, my uuu tool hang at:

sudo uuu -b nand u-boot-nand-2020.04-r0.imx
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.107-15-gd1c466c

Success 0 Failure 0

1:21 1/ 1 [=================100%=================] SDP: boot -f u-boot-nand-2020.04-r0.imx

And at my board, the console hang at:

U-Boot 2020.04-imx_v2020.04_5.4.24_2.1.0+g4979a99482 (Mar 19 2021 - 08:33:56 +0000)

CPU: i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 43C
Reset cause: POR
Model: i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 256 MiB
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from NAND... *** Warning - bad CRC, using default environment

Display: ILI9488-QVGA (480x320)
Video: 480x320x24
Error: no valid bmp image at 8c000000

Do you have any idea for this? Thanks for your help.
Thanks,
Quyet Luu

0 Kudos
Reply
1 Solution
1,361 Views
91_quyetluu
Contributor II

When i cropped the logo from 480x320 down the smaller size. The process is done. Do you guy have any information about? Thanks

Thanks,
Quyet Luu

View solution in original post

0 Kudos
Reply
1 Reply
1,362 Views
91_quyetluu
Contributor II

When i cropped the logo from 480x320 down the smaller size. The process is done. Do you guy have any information about? Thanks

Thanks,
Quyet Luu

0 Kudos
Reply