UUU : Fail Bulk(R):LIBUSB_ERROR_IO(0.017s)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UUU : Fail Bulk(R):LIBUSB_ERROR_IO(0.017s)

1,813件の閲覧回数
rakesh3
Contributor V

Hi team,

I am using the UUU version 1.5.21 and while flashing the image to imx6qsabresd board where I am using the saveenv command. I am getting the below error .

New USB Device Attached at 1:9
1:9>Start Cmd:SDP: boot -f u-boot-dtb.imx
100%1:9>Okay (1.284s)
New USB Device Attached at 1:9
1:9>Start Cmd:FB: ucmd setenv fastboot_dev mmc3
1:9>Okay (0.001s)
1:9>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
1:9>Okay (0s)
1:9>Start Cmd:FB: ucmd saveenv
1:9>Fail Bulk(R):LIBUSB_ERROR_IO(0.017s)

Below is my UUU script for loading the u-boot.

 

uuu_version 1.5.21

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f u-boot-dtb.imx

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f u-boot-dtb.imx

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f u-boot-dtb.imx -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f u-boot-dtb.imx -skipspl
SDPV: jump
# }

# use uboot burn bootloader to eMMC
# becaue difference chip, offset is difference
# you can use kernel to do that for specific boards
FB: ucmd setenv fastboot_dev mmc3
FB: ucmd setenv mmcdev ${emmc_dev}

FB: ucmd saveenv
FB: flash bootloader u-boot-dtb.imx

FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;

FB: ucmd setenv emmc_cmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0

FBK: DONE

 

Please help me to find the issue on the mentioned error .

Regards,

RK

ラベル(3)
0 件の賞賛
返信
1 返信

1,786件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @rakesh3,

 
I hope you are doing well
 
As the same query is raised in another thread and the communication is ongoing in the previous thread I would request to close this case. 
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信