UTP: sending Non-success to kernel for command $ echo 0 > /sys/block/mmcblk0boot0/force_ro.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UTP: sending Non-success to kernel for command $ echo 0 > /sys/block/mmcblk0boot0/force_ro.

2,636件の閲覧回数
rheehans
Contributor I

hi all

I did binary programming in emmc that connected SD4 with MFC Tool, but I did not succeed as below image...

mkc_tool.png

debug message is

========================================

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)

to zero the first 512 bytes:  dd if=/dev/zero of=/dev/foo7 bs=512 count=1

(See fdisk(8).)

UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk0.

utp_poll: pass returned.

UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129'

UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129"

129+0 records in

129+0 records out

UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129.

utp_poll: pass returned.

UTP: received command '$ echo 0 > /sys/block/mmcblk0boot0/force_ro'

UTP: executing "echo 0 > /sys/block/mmcblk0boot0/force_ro"

sh: /sys/block/mmcblk0boot0/force_ro: No such file or directory

UTP: sending Non-success to kernel for command $ echo 0 > /sys/block/mmcblk0boot0/force_ro.

==========================================================

======================= mfctool.log ===========================

ModuleID[2] LevelID[10]: DeviceTypeDisk--_devices size: 7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:8, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:2, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:3, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:4, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:5, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:6, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:7, Volume->_diskNumber:7

ModuleID[2] LevelID[10]: DeviceTypeDisk--find Disk device: 008EA078

ModuleID[2] LevelID[10]: Device::hubIndex::getmsc, return the port index is: 1

ModuleID[2] LevelID[10]: VolumeDeviceClass::AddUsbDevice() successful L add to current list, retrycount: 0

ModuleID[2] LevelID[10]: Device::hubIndex::getmsc, return the port index is: 1

ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - VOLUME_ARRIVAL_EVT-Disk(L), Hub:3-Port:1

ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - VOLUME_ARRIVAL_EVT, Notify

ModuleID[2] LevelID[10]: CmdOpreation[0]--OnDeviceChangeNotify, Volume Arrive/Remove or Device Arrive/Remove

ModuleID[2] LevelID[10]: CmdOpreation[0]--OnDeviceChangeNotify, m_p_usb_port is not NULL, so only refresh

ModuleID[2] LevelID[10]: CmdOpreation[0]--OnDeviceChangeNotify, Volume/Device Arrive

ModuleID[2] LevelID[1]: CmdOpreation[0]--set m_hDeviceArriveEvent.

ModuleID[2] LevelID[10]: CmdOpreation[0]--WaitforEvents device arrive1

ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 1

ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is send

ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ tar xf $FILE

ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ sh mksdcard.sh /dev/mmcblk0

ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ dd if=/dev/zero of=/dev/mmcblk0 bs=1k seek=384 conv=fsync count=129

ModuleID[2] LevelID[10]: ExecuteCommand--Push[WndIndex:0], Body is $ echo 0 > /sys/block/mmcblk0boot0/force_ro

ModuleID[2] LevelID[1]: PortMgrDlg(0)--MSCDevice--Command Push(no file) excute failed

ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - DEVICE_ARRIVAL_EVT(\\?\USB#VID_0480&PID_0200#20140525005600F#{a5dcbf10-6530-11d2-901f-00c04fb951ed})

ModuleID[2] LevelID[10]: DeviceManager::DevChangeWnd::OnDeviceChange() - end

=============================================================

please recommand about this error...

ラベル(2)
0 件の賞賛
返信
1 返信

1,781件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rhee

if this is custom board, then MFG Tool should be rebuild according to

board configuration, below link with similar problem

use mfgtool download imx6ql eMMC error | Freescale Community

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信