USB2.0 Compliance test (Android)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB2.0 Compliance test (Android)

1,882 Views
yuhigashino
Contributor I

Hi

I'm developing Embedded Board with i.MX6 Quad in Android (KitKat).

For the USB 2.0 HS compliance test of HOST, tested Board have to generate test packet.

But, I don't know the way.

 

Is there any recommend way for that?

 

if there is, please let me know.

 

thanks

0 Kudos
Reply
1 Reply

1,540 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yu

usb test mode for compliance test can be implemented using memtool kitkat patch

android-imx6-kitkat/0347-ENGR00222875-1-Lindent-memtools.patch at master · rabeeh/android-imx6-kitka... 

Patch to make i.MX6DQ USB to support test modes for certification test 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply