USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB

2,331件の閲覧回数
Ajayvk
Contributor I

I have the USB hub which is controlled by the PIN71 USB2_EN_OC# i need to implement the USB2_EN_OC# to be low all the time so for that we are not able to figure out the pad mux by which we can make it low we are using IMX8MPLUS board so please give us a solution for it

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,289件の閲覧回数
Ajayvk
Contributor I

Ajayvk_0-1705907400966.png

this is the pin which i need to make low all the time so how can i make it low all the time in imx8mp dts im not able to see how this is mapped so that i can make it low so power will be disabled

0 件の賞賛
返信

2,280件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

You didn't mentioned that you used SECO SOM, but found this user manual.

josephlinares_0-1705959811618.png

I can infer that that signal is related to Cypress USB3304-68LTXC USB 3.0 hub controller or its control circuit and the carrier board should implement a pulled-up resistor to 3.3V_RUN signal or GROUND as per your request; I don't think it's mapped to processor, I'm sending you a private mail to discuss further.

Regards,

0 件の賞賛
返信

2,305件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Could you clarify if my understanding is alright? You would like to use a pin pulled low from i.MX 8M Plus EVK.

Then, you should reserve the pin in device tree, this guide can accomplish the whole process. And to choose a pin, you could use UART3 TXD or RXD but disable it on device tree.

josephlinares_0-1705788374850.png

Regards

0 件の賞賛
返信