USB isochronous transfer queries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB isochronous transfer queries

1,443 Views
binaeksarkar
Contributor II

Hi,

I have some queries regarding usb isochronous endpoint operation for device controller. I am referring to the document "IMX6DQRM-Rev1.pdf" section 65.4.5.

1. During an isochronous in transfer, does Dqh contain only one Dtd which has only one  Iso (micro)frame or does Dqh contain one or multiple linked Dtds which has an input buffer filled with many iso frame/microframe? If multiple then how does device controller identify (micro)frame boundaries in dtds?

2. Is there any DMA operation involved while moving data between DTD and TX/RX FIFO? If DMA is present then what is the DMA restriction of buffer size and start address alignment?

Thanks

Barindam

Labels (1)
0 Kudos
Reply
1 Reply

1,280 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Barindam,

Could you please specify if you still having these queries or you are already on the stage mentioned on your other thread?

Additionally, you could take a look to application note AN4589 “Configuring USB on i.MX 6 Series Processors”, which provides useful information regarding USB on i.MX6 series.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply