USB init failed -19 in uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB init failed -19 in uboot

1,841 次查看
venu_mos
Contributor II

Hi NXP Community,

Iam currently working on fastboot for imx8mp board phyboard pollux board, but whenever i try to unlock the bootloader it return an error message i will attach screen shots below to better describe my problem here,

whenever i try booting from u-boot i get some other error messages like "usb init failed -19"

venu_mos_0-1691041511088.png

 

 

please find the attached images to better understand the problem

venu_mos_1-1691041511112.png

 

my goal is to flash images to the board in fastboot mode

@weidong_sun 

0 项奖励
回复
1 回复

1,806 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @venu_mos 

The second attached image ambiguous, and the first is part of log. 

As below are your scenarios?

Solved: [IMX8MP] uuu download stuck and "USB init failed: ... - NXP Community

Re: iMX8MQ UUU tool error - NXP Community

Solved: MX8MM won't enter fastboot mode - NXP Community

And refer to the attachment for a patch which enable uuu on none type c board.

 

Best regards

Harvey

0 项奖励
回复