USB host control transfer data toggle problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB host control transfer data toggle problem

2,636件の閲覧回数
FredrikMoller
Contributor III

Background info: I'm writing a host controller driver for the i.MX28EVK.

Problem: When reading from device (i.e. the data phase of the control transfer is an IN transaction), host sends a DATA0 packet in the status phase. According to the USB 2.0 standard ch. 8.5.3, this should be a DATA1 packet. Is this a hardware issue? Is there any way to work around or solve the issue?

ラベル(1)
0 件の賞賛
返信
1 返信

2,376件の閲覧回数
FredrikMoller
Contributor III

It was an error in my code. Hardware is fine. I relied on automatic data toggling which caused the controller hardware to toggle the data toggle from DATA1 (data phase) to DATA0 (status phase).

0 件の賞賛
返信