USB error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB error

2,244件の閲覧回数
mohammedazlum
Contributor IV

When board is booting [Linux BSP], I'm getting below USB error. Please share your feedback.

usb 2-1.3: device descriptor read/64, error -32

usb 2-1.3: new low speed USB device number 33 using fsl-ehci

usb 2-1.3: device descriptor read/64, error -32

usb 2-1.3: device descriptor read/64, error -32

usb 2-1.3: new low speed USB device number 34 using fsl-ehci

usb 2-1.3: device not accepting address 34, error -32

usb 2-1.3: new low speed USB device number 35 using fsl-ehci

usb 2-1.3: device not accepting address 35, error -32

hub 2-1:1.0: unable to enumerate USB device on port 3

Regards,

Azlum

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,779件の閲覧回数
mohammedazlum
Contributor IV

Dear Yuri,

Let me try as you suggested.

Regards,

Azlum

0 件の賞賛
返信

1,779件の閲覧回数
Yuri
NXP Employee
NXP Employee

   You may try the following, at least, to clarify the issue :

1.

  Using external self-powered USB hub .

2.

  Check USB design. Please refer to section 3.11 (USB recommendations) of IMX6DQ6SDLHDG 


“Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …”


http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信