USB dual role patch for Linux 3.10.17 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB dual role patch for Linux 3.10.17 BSP

ソリューションへジャンプ
10,450件の閲覧回数
Henry_p
NXP Employee
NXP Employee

CPU: i.MX6 solo

BSP version: 3.10.17

Application: Car AVN

My customer wants to implement iOS Carplay solution for his product.

Could you help me to get USB dual role patch for USB driver in 3.10.17 BSP?

ラベル(3)
1 解決策
8,537件の閲覧回数
Henry_p
NXP Employee
NXP Employee

Please find the attachment.

元の投稿で解決策を見る

6 返答(返信)
8,537件の閲覧回数
Henry_p
NXP Employee
NXP Employee

Got a patch from SH AE team.

0 件の賞賛
返信
8,537件の閲覧回数
brucecollie
Contributor I

Hi,

Would it be possible for you to share the patch you received, or to put me in contact with the people you received the patch from?

Thanks

0 件の賞賛
返信
8,538件の閲覧回数
Henry_p
NXP Employee
NXP Employee

Please find the attachment.

8,537件の閲覧回数
shravansundarra
Contributor I

Dear Henry.p‌,

Is similar patch available for kernel version 4.1.15-1.2.0 ?

I have posted a query in this thread.

Thanks

0 件の賞賛
返信
8,537件の閲覧回数
huipingping
Contributor I

another problem: (Android 5.0)Patch code for i.MX6Q failed. c_patch does't work

We want to run android 5.0 on our I.MX6Q. We download the source code,freescale kernel,U-boot,path. Following the Android User's Guide, we now having a problem when patching. After running source /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga/and_patch.sh and enters help, it shows this:

Invoke ". and_patch.sh" from your shell to add following functions to your enviroment:

-- c_gotop:  Change directory .....

-- c_patch:  Recover working tree...

Then, running c_patch /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga imx_l5.0.0_1.0.0-ga does't work. It shows c-patch: commond not found. Why c_patch does't work? Was it really add c_patch function sucessfully when running “  source /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga/and_patch.sh”. How can we patch sucessfully?

Thank you

0 件の賞賛
返信
8,532件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yong

dual-role mode (otg) is implemented in chipidea usb driver,

refer to Linux Manual sect.41.2.6 Changing the Controller Operation Mode,

controller mode is defined at dt file, eg arch/arm/boot/dts/imx6q-sabresd.dts

dr_mode =  “otg” /* Set controller as otg mode */

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信