USB controller: Which field is the adress destination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB controller: Which field is the adress destination

Jump to solution
1,284 Views
alexandredel
Contributor I

Hello

I'm working on the USB controller of the IMX 6Quad and i don't understand something. I read the documentation named "Application Processor Reference Manual", chapter 65, page 5270, but i don't find which field set up the adress destination for an iTD.

Is it the buffer pointer? Does someone knows this information? Or can help me to find it?

Thanks

Alexandre

Labels (1)
0 Kudos
Reply
1 Solution
1,194 Views
Yuri
NXP Employee
NXP Employee

Yes, - the buffer pointer.

Note, new Reference Manual release (IMX6DQRM, Rev 2, 06/2014) is available now.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,195 Views
Yuri
NXP Employee
NXP Employee

Yes, - the buffer pointer.

Note, new Reference Manual release (IMX6DQRM, Rev 2, 06/2014) is available now.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply