USB class support in iMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB class support in iMX6

1,103 次查看
krunalk
Contributor II

Hi,

Does the iMX6ULL support,

1. HID and VCP class in the USB Host mode?

2. HID and VCP class in the USB Device mode?

I am confused because in the " i.MX Linux® Release Notes, Rev. L4.1.15_2.0.0-ga, 10/2016" Page-14, in USB section, they mentioned " USB device mode: MSC, Ethernet, and Serial" only.

Please guide.

Thanks.

标记 (2)
0 项奖励
回复
2 回复数

853 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Krunal,

The USB driver available in the Linux BSP  L4.1.15_2.0.0-ga  supports   USB Class HID  in HOST and Device mode.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

853 次查看
krunalk
Contributor II

Thanks Jamesbone,

Then why they have mentioned only MSC, Ethernet and Serial class in  " i.MX Linux® Release Notes, Rev. L4.1.15_2.0.0-ga, 10/2016" Page-14, in USB device section? Is there any limitations?

I am asking because USB HID class is important for me in both USB DEVICE and HOST mode. iMX is a host platform and supports both keyboard, mice so I have no doubt for HID support in Host mode. But I want to make sure that it also supports HID class in device mode.

Thanks again.

0 项奖励
回复