USB Video class Composite Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Video class Composite Device

1,724 Views
Ismael_dz
Contributor II

Hello community! I got a question. For a UVC composite device with Color and sensor Camera, do I need more than 1 Video Control Descriptor? Im not sure If I simply can add the inteface and endpoint for the second camera and still use one video control of if it is needed to use two video control descriptor.

0 Kudos
Reply
1 Reply

1,706 Views
kef2
Senior Contributor V

Hello, Ismael_dz 

Do you mean UVC class device streaming two videos simultaneously? UVC class allows many video sensors (sources) in one device but streaming just a single one at a time. Selector interface allows switching among sources. But there are no means to define two or more simultaneous video streams. That's for standard UVC device, which is recognized by built-in Windows driver.  

0 Kudos
Reply