USB Serial Downloader mode - IMX6 Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Serial Downloader mode - IMX6 Quad

4,590 Views
rajniks
Contributor I

I have a custom board design in which USB Serial down-loader mode doesn't seem to work. I have been able to connect Lauterbach debugger directly but have not been successful with serial downloader mode.

On my board, I have connected USB_OTG_ID to pin T4 which has ALT3 functionality as OTG_ID. Will this create a problem as I can see on Sabre Smart OTG_ID is connected to Pin W23 which has ALT0 functionality as OTG_ID. Please let me know if the Freescale internal boot code looks only at one of these in order to decide to boot as USB device or host mode.

Labels (2)
0 Kudos
Reply
8 Replies

3,633 Views
cameronmadsen
Contributor I

Raj, on the off chance you see this, did you ever resolve the issue? We have a custom Dual board and are seeing the exact same behavior.

0 Kudos
Reply

3,633 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raj

iROM code does not check OTG_ID.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,633 Views
rajniks
Contributor I

Hello,

The problem on my custom board looks like the processor is not going into correct boot mode by switch setting. I initially had a 10K pull down and switch to connect 3.3V. While experimenting when I pull down both the lines to low which is actually "boot from fuses mode" my board gets detected as USB Device and I am able to connect DDR Tester software.

When I try to configure the serial downloader mode by setting boot mode pin 0 as 3.3V and  pin 1 as pull down nothing happens.

Why would such a problem exists. I have checked the state of both the boot  options and they seem to be at good level when the POR is deasserted. I am getting stuck with this issue and any pointers will be quite helpful.

0 Kudos
Reply

3,633 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raj

you can check what boot mode is used by processor reading

SRC Boot Mode Register (SRC_SBMR2), SRC_SBMR1.

Best regards

chip

0 Kudos
Reply

3,633 Views
rajniks
Contributor I

Hi Igor,

I am trying to read both registers using lauterbach T32. I am able to see BMOD value changing in the SBMR2 as per my switch settings but SBMR1 remains 0. Is this okay or we are messing something up here?

Regards

Raj 

0 Kudos
Reply

3,633 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raj

in serial mode SBMR1 may be not read.

Probably boot signals are connected (shorted) on board internally to smth.

which causes this beahviour. Is it one board only ?

Is it possible to solder board with minimal set of components and check.

Best regards

igor

0 Kudos
Reply

3,633 Views
rajniks
Contributor I

I am seeing this behavior on two boards that we have built. I am not suspecting any inadvertent shorts as SBRM2 values changes as per the setting done by the switches.

0 Kudos
Reply

3,633 Views
igorpadykov
NXP Employee
NXP Employee

Two boards among what "N" ?

I think you can change processor from good board to

problem board (and vice versa) and check.

0 Kudos
Reply