USB SD Card detect insertion?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB SD Card detect insertion?

2,773件の閲覧回数
adamwolf
Contributor I

Hi folks,

I have a USB SD card reader on an i.MX6, running Android.  I am trying to get the kernel to detect when a card is inserted.  Right now, it properly detects the card only if it is plugged in before the USB reader is plugged into the system.

I have tested the behavior on multiple PCs, and the USB SD card reader behaves as expected.

In Android, mounting is controlled by vold.  vold appears to be working correctly, so I enabled extra logs so I see all netlink/uevents that are produced.

When I plug in the reader, /sys/class/block/sda shows up regardless of if a device is in it—that is expected.  Then, when I insert a card, I get no uevent.  I echoed 2000 into /sys/module/block/parameters/events_dfl_poll_msecs, and now when I insert a card (and wait about 2 seconds), I get an event:

DEVPATH=/devices/blah/blah/blah/block/sda

DISK_MEDIA_CHANGE=1

MAJOR=8

MINOR=32

DEVNAME=sda

DEVTYPE=disk

NPARTS=0

There are no further events after that.

All of that looks fine, except… NPARTS=0!?!?!  The card has one partition, and if I unplug the reader, insert the card into the reader, and plug the reader in, I get

DEVPATH=/devices/blah/blah/blah/block/sda

MAJOR=8

MINOR=32

DEVNAME=sda

DEVTYPE=disk

NPARTS=1

I expect additional events, like a block->disk event and a block->partition event after block->DISK_MEDIA_CHANGE.


Is this something I need to configure?  If not, if this is something that is simply not supported, I believe I need to set it up so that on DISK_MEDIA_CHANGE, the kernel also rescans for partitions.  Any thoughts on where to do it?  I see code like that in block/sd.c, fs/block_dev.c, and fs/genhd.c.  (A USB SD card reader touches lots of parts of the kernel!)

Thanks!

ラベル(3)
0 件の賞賛
返信
1 返信

1,977件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

I think the problem you are having it is in the USB more than in the SD Card drvier itself, do you have a Log, so we can review how the device it is enumerated, do you have an schematic of the USB part to see how is the OTG or it is in a FSL board?,  If you can use a USB Sniffer to see what it is happening when you plug the SD would be great.

0 件の賞賛
返信