USB OTG IMX8MPlus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB OTG IMX8MPlus

跳至解决方案
6,704 次查看
ChienNQ
Contributor II

How to design USB micro for IMX8MPlus?

How to Implement usb otg without USB ID? 

I did not find the ID pin on the IMX8Mplus, on the datassheet documentation, please support? Can i use any GPIO for detect function? 

0 项奖励
回复
1 解答
6,574 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ChienNQ,

USB1_ID pin muxing is available on GPIO1_IO10 only. One can check the same from the Config Tools for i.MX Applications Processors.

Thanks & Regards,
Ritesh M Patel

在原帖中查看解决方案

0 项奖励
回复
7 回复数
6,666 次查看
ChienNQ
Contributor II

Thanks for great support

0 项奖励
回复
6,678 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ChienNQ,

I hope you are doing well.

The USBx_ID is muxed with GPIO. One can refer to Page 1350 of i.MX8MP Reference Manual.
USB1_ID --> GPIO1_IO10
USB2_ID --> GPIO1_IO11

To implement the USB OTG functionality without USB-C, one can refer to the below-mentioned link which is valid for i.MX8MP as well.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-US...

I hope it helps.

Thanks & Regards,
Ritesh M Patel

6,610 次查看
ChienNQ
Contributor II

Hi @riteshmpatel ,

Thanks for support. 

We build our device form compulab SOM UCM-iMX8PLUS . 

And they did not connect GPIO1_IO10 to SOM. Can i use another GPIO like GPIO1_0 for ID function?

Please see this link for more detail https://www.compulab.com/wp-content/uploads/2022/03/ucm-imx8plus_reference-guide_2023-01-12.pdf

Thanks and best regards,

 

0 项奖励
回复
6,575 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ChienNQ,

USB1_ID pin muxing is available on GPIO1_IO10 only. One can check the same from the Config Tools for i.MX Applications Processors.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复
6,528 次查看
ChienNQ
Contributor II

Hi @riteshmpatel ,

Thanks for support us. 

One more question, in case IMX8MP Plus is in bootloader mode, is it always in device mode? and regardless of the state of the ID?

Thanks and best regards,

Trend Nguyen

0 项奖励
回复
6,661 次查看
khang_letruong
Senior Contributor III
0 项奖励
回复
6,600 次查看
ChienNQ
Contributor II

Thanks @khang_letruong 

0 项奖励
回复