USB_Host_CDC not working properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB_Host_CDC not working properly

Jump to solution
934 Views
smartpavan333
Contributor I

Hi,

I am working on IMXRT1170-EVK and I took the example of "USB_Host_CDC".

(Note : I had a another board IMXRT1064-EVK configured as USB_Device and took the Example of "USB_Device_CDC_Vcom").

Q1 : When I ran the SDK  I am able get the data for every 10ms over USB_Host_cdc , after some time SDK code getting Crashed.

Q2: Any hardware changes are required for High speed on USB ?

Can you help me this issue?

0 Kudos
Reply
1 Solution
850 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @smartpavan333 ,

I made a same test, RT1170EVK+RT1050EVKB. It works fine. The RT1170EVK doesn't crash after a long time. Did you change anything? I think there is no hardware change required for high speed, the demo is high speed mode by default.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
851 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @smartpavan333 ,

I made a same test, RT1170EVK+RT1050EVKB. It works fine. The RT1170EVK doesn't crash after a long time. Did you change anything? I think there is no hardware change required for high speed, the demo is high speed mode by default.

 

Regards,

Jing

0 Kudos
Reply