USB Diagnostic information for Bit Error Rate Analysis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Diagnostic information for Bit Error Rate Analysis

1,451件の閲覧回数
rreddy
Contributor I

We are using the i.MX6 Dual processor in a custom design that utilizes the USB Device, USB Host1 (UTMI) and USB Host2 (HSIC) ports.  Does the iMX6 USB PHY provide diagnostic registers for the purpose to tracking recovered error quantities, types, etc. in the interest of being able to compute the BER of the link physical?

ラベル(2)
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rakesh

I am afraid there are no registers showing error quantities.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信