USB Diagnostic information for Bit Error Rate Analysis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Diagnostic information for Bit Error Rate Analysis

1,503 Views
rreddy
Contributor I

We are using the i.MX6 Dual processor in a custom design that utilizes the USB Device, USB Host1 (UTMI) and USB Host2 (HSIC) ports.  Does the iMX6 USB PHY provide diagnostic registers for the purpose to tracking recovered error quantities, types, etc. in the interest of being able to compute the BER of the link physical?

Labels (2)
0 Kudos
Reply
1 Reply

1,454 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rakesh

I am afraid there are no registers showing error quantities.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply