USB Communication between to self powered boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Communication between to self powered boards

3,014 Views
DSEngineer
Contributor I

Hi Everyone,
I'm working on a design and I'm not sure it will work properly.
Mainly because the USB is OTG and there is no VBUS connection between the boards.
I want to make a connection between two boards, each board has it's own power supply, there is no VBUS connection between the boards. One board will function as a master and the other as a device.
Does anyone have suggestions for repair/addition or advice on how to do it better?
I added a picture to illustrate the connection between the boards.

Labels (1)
0 Kudos
Reply
3 Replies

2,993 Views
DSEngineer
Contributor I

Hi Igor,
Thanks for the help.
Yes, I was thinking about this configuration, but when one is set as a device he does not expect to get 5V in VBUS? Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?

0 Kudos
Reply

2,991 Views
igorpadykov
NXP Employee
NXP Employee

>Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?

 

on device side VBUS can be connected directly to 5V.

 

Best regards
igor

0 Kudos
Reply

3,002 Views
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

 

for communication between two boards one can try to use usb unit tests, configure

one board as host other as device:

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=lf-5.10.52_2.1.0

 

Best regards
igor

0 Kudos
Reply