USB Communication between to self powered boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Communication between to self powered boards

2,989件の閲覧回数
DSEngineer
Contributor I

Hi Everyone,
I'm working on a design and I'm not sure it will work properly.
Mainly because the USB is OTG and there is no VBUS connection between the boards.
I want to make a connection between two boards, each board has it's own power supply, there is no VBUS connection between the boards. One board will function as a master and the other as a device.
Does anyone have suggestions for repair/addition or advice on how to do it better?
I added a picture to illustrate the connection between the boards.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,968件の閲覧回数
DSEngineer
Contributor I

Hi Igor,
Thanks for the help.
Yes, I was thinking about this configuration, but when one is set as a device he does not expect to get 5V in VBUS? Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?

0 件の賞賛
返信

2,966件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?

 

on device side VBUS can be connected directly to 5V.

 

Best regards
igor

0 件の賞賛
返信

2,977件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

 

for communication between two boards one can try to use usb unit tests, configure

one board as host other as device:

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=lf-5.10.52_2.1.0

 

Best regards
igor

0 件の賞賛
返信