USB Camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Camera

3,702件の閲覧回数
1182614726
Contributor III

大家好,

            我目前使用imx6solo芯片,linux版本为L4.1.15,使用yocto编译的BSP版本为fsl-yocto-L4.1.14_2.0.0-ga。目前有个USB摄像头需求。

            1.考虑到imx6solo带有VPU视频编解码,请问这个要怎么才能用起VPU呢?

            2.我们USB摄像头目前仅支持两种格式:MJPEG和YUV422。对于imx6solo的VPU可以对我们目前的两种格式进行解码吗?

ラベル(1)
3 返答(返信)

3,428件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

About your above questions, the default BSP support the VPU encoding, you can directly use. The i.mx6solo support encording H264, MPEG4, MJPEG, but when go to the vpu, only support the YUV420. Yes, as you said, you can use the gstreamer.


0 件の賞賛
返信

3,428件の閲覧回数
1182614726
Contributor III

另外,有建议使用gstreamer显示usb摄像头,请问要如何实现呢?谢谢

3,428件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About how the use the GStreamer you can refer to :Using a USB Camera with GStreamer
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信