USB 3 Polarity Inversion TX and RX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 3 Polarity Inversion TX and RX

Jump to solution
6,072 Views
MNTR
Contributor I

Hello,

according to the USB3 spec it is allowed to invert the polarity of the USB_TX or USB_RX signals without any further adjustments.

Since we got some issues with our USB-Interface where we inverted USB2_TX_N and USB2_TX_P as well as USB2_RX_N and USB2_RX_P, I want to make sure this is allowed with the i.MX8M Plus.

Can anybody confirm this inversion is possible and we do not have to adjust any settings or similar?

IMX8MPLUS 

0 Kudos
Reply
1 Solution
6,046 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

TX/RX polarity inversion is supported on i.MX8MP.

USB 3.0 PHY has auto polarity detection and adjustment support.

Thanks & Regards,
Dhruvit Vasavada

 

View solution in original post

3 Replies
6,030 Views
MNTR
Contributor I

Hi @Dhruvit ,

thank you very much. 
Are there any limitations? 
For example: can I invert just one of the super speed pairs (TX inverted, RX not inverted)? 

Thanks in advance

0 Kudos
Reply
5,981 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

i.MX8MP has Synopsys USB 3.0 PHY.

Lane Polarity inversion only talks about Rx signals.

Please refer to Universal Serial Bus 3.0 Specification for more information.

Thanks & Regards,
Dhruvit Vasavada

6,047 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @MNTR,

I hope you are doing well.

TX/RX polarity inversion is supported on i.MX8MP.

USB 3.0 PHY has auto polarity detection and adjustment support.

Thanks & Regards,
Dhruvit Vasavada