USB 3.1 Gen 2 Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 3.1 Gen 2 Support

1,729 Views
erwin_wolniewit
Contributor III

When in the roadmap does NXP will start to offer USB 3.1 gen 2 host and device?

Tags (2)
0 Kudos
Reply
1 Reply

1,659 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Erwin,
There are no plans yet to include USB 3.1 (in terms of speed transfers) on i.MX processors. USB 3.0 was included starting i.MX8 series of i.MX processors.
In terms of other compatibility, you could add Power Delivery and USB-C connector with current USB 3.0 controller, like the implementation on the i.MX8 MEK and EVK boards.
For additional parts related to USB-C or USB 3.1, you could take a look to the following links:

USB Type-C and Power Delivery Evaluation Kits | NXP 

PTN36502 - Type-C USB 3.1 Gen 1 and DisplayPort v1.2 combo redriver | NXP 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply