UDP broadcast failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UDP broadcast failed

Jump to solution
7,013 Views
小川崇
Contributor II

Greetings,

I made UDP broadcast program as shown below.
I ran the program on i.MX6 board.
but sendto() always reterun -1.

i.MX6 board is setup with IP address 192.168.0.1, subnet 255.255.255.0.

I want to fix this error.
but I don't know how to fix this problem.
I appreciate if someone can help me to solve it

Regards,

takashi


#include <sys/types.h>
#include <sys/socket.h>
#include <netinet/in.h>
#include <stdio.h>

int
main()
{
int sock;
struct sockaddr_in addr;
int yes = 1;
int ret;
int opt;

sock = socket(AF_INET, SOCK_DGRAM, 0);
if(sock < 0)printf("socket() failed!!\n");

addr.sin_family = AF_INET;
addr.sin_port = htons(8503);
addr.sin_addr.s_addr = inet_addr("255.255.255.255");

opt = setsockopt(sock,SOL_SOCKET, SO_BROADCAST, (char *)&yes, sizeof(yes));
if(opt < 0)printf("setsockopt() failed!!\n");

ret = sendto(sock, "HELLO", 5, 0, (struct sockaddr *)&addr, sizeof(addr));
if(ret!=5)printf("sendto() failed!!\n");


close(sock);

return 0;
}

Labels (2)
1 Solution
5,802 Views
BrilliantovKiri
Senior Contributor I

I think your system havn't routing to destination network.

Because you try send packet on broadcast address I think you solve probleam

after configuration default gateway.

View solution in original post

0 Kudos
Reply
5 Replies
5,810 Views
BrilliantovKiri
Senior Contributor I

Hello!

1. check errno variable after sendto

2. your system should have route to destination network

5,810 Views
LeonardoSandova
Specialist I

In addition, if you can use strace to run your app, you will find more insight. To print the error with useful info, use strerror(errno) and do it just after the call to sendto (this variable is global, so any system call modify it).

Leo

5,810 Views
小川崇
Contributor II

Hi

I checked errno and error reason by using strerror.

error no. is 101:Network is unreachable.

What does error no. 101 mean?

What is the problem?

takashi

0 Kudos
Reply
5,803 Views
BrilliantovKiri
Senior Contributor I

I think your system havn't routing to destination network.

Because you try send packet on broadcast address I think you solve probleam

after configuration default gateway.

0 Kudos
Reply
5,810 Views
小川崇
Contributor II

Hi

after I set default gateway  I ran the program.

sendto returned 5.

The error did not occur.

Thank you for your advice.

takashi

0 Kudos
Reply