UDP broadcast failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UDP broadcast failed

跳至解决方案
6,657 次查看
小川崇
Contributor II

Greetings,

I made UDP broadcast program as shown below.
I ran the program on i.MX6 board.
but sendto() always reterun -1.

i.MX6 board is setup with IP address 192.168.0.1, subnet 255.255.255.0.

I want to fix this error.
but I don't know how to fix this problem.
I appreciate if someone can help me to solve it

Regards,

takashi


#include <sys/types.h>
#include <sys/socket.h>
#include <netinet/in.h>
#include <stdio.h>

int
main()
{
int sock;
struct sockaddr_in addr;
int yes = 1;
int ret;
int opt;

sock = socket(AF_INET, SOCK_DGRAM, 0);
if(sock < 0)printf("socket() failed!!\n");

addr.sin_family = AF_INET;
addr.sin_port = htons(8503);
addr.sin_addr.s_addr = inet_addr("255.255.255.255");

opt = setsockopt(sock,SOL_SOCKET, SO_BROADCAST, (char *)&yes, sizeof(yes));
if(opt < 0)printf("setsockopt() failed!!\n");

ret = sendto(sock, "HELLO", 5, 0, (struct sockaddr *)&addr, sizeof(addr));
if(ret!=5)printf("sendto() failed!!\n");


close(sock);

return 0;
}

标签 (2)
1 解答
5,446 次查看
BrilliantovKiri
Senior Contributor I

I think your system havn't routing to destination network.

Because you try send packet on broadcast address I think you solve probleam

after configuration default gateway.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
5,454 次查看
BrilliantovKiri
Senior Contributor I

Hello!

1. check errno variable after sendto

2. your system should have route to destination network

5,454 次查看
LeonardoSandova
Specialist I

In addition, if you can use strace to run your app, you will find more insight. To print the error with useful info, use strerror(errno) and do it just after the call to sendto (this variable is global, so any system call modify it).

Leo

5,454 次查看
小川崇
Contributor II

Hi

I checked errno and error reason by using strerror.

error no. is 101:Network is unreachable.

What does error no. 101 mean?

What is the problem?

takashi

0 项奖励
回复
5,447 次查看
BrilliantovKiri
Senior Contributor I

I think your system havn't routing to destination network.

Because you try send packet on broadcast address I think you solve probleam

after configuration default gateway.

0 项奖励
回复
5,454 次查看
小川崇
Contributor II

Hi

after I set default gateway  I ran the program.

sendto returned 5.

The error did not occur.

Thank you for your advice.

takashi

0 项奖励
回复