UBOOT Code Development

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UBOOT Code Development

2,147件の閲覧回数
DogZapper
Contributor I

I am an "old school" embedded hardware geek... In my world real men write all firmware from scratch using "C"... (or at least start from hello_world.c found in some eval kit)  I'm totally lost in the Linux world...

Where is my jtag debugger and where do I plug it in.  I'm ready to fire up the IDE in Eclipse and download some code...

I have inherited an EPD based system designed by someone else, using bits and pieces of the iMX508 EVK design.  What I would like to do is learn how to write UBOOT code... That seems like the world I'm comfortable in.

I have another colleague working on the Linux stuff... My job is to verify that the HW is working right and help with software if he gets desperate.

Unfortunately, I do not have access to an iMX508 EVK right now... only the HW based on the EVK...

Someone point me in the right direction to start UBOOT code development.  Do I need to purchase a compiler from Freescale or do I just use the Linux compiler stuff for UBOOT development.

The HW I have right now runs a version of UBOOT from a plug-in SD card.  I need to add some additional commands of my own.  Unfortunately, right now, I do not have access to this source code...I'm working on getting it...

Can I download a version of UBOOT source code for the iMX508 EVK and start from there?

Signed...

At the bottom of the learning curve... looking up for help...

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,863件の閲覧回数
DogZapper
Contributor I

I found some stuff here...

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX508&fpsp=1&tab=Documentation_Tab

IMX50_1104_LINUXDOCS_BUNDLE  
Includes EVK Linux Hello World App Note, Read Me Doc, Release Notes, Reference Manual and User's Guide

After, downloading the tar ball... unzipping it, I found the PDF file...  uboot_mx5x.pdf.... This looks like the place for me to start...  sweet...

0 件の賞賛
返信