UBI error: process_eb: bad image sequence number

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UBI error: process_eb: bad image sequence number

6,290件の閲覧回数
moseeneview
Contributor II

I get the below UBI error when kernel startup.

i.MX6q + anddroid 4.3

it occurs at UBI scan (drivers/mtd/ubi/scan.c)

Then the system doesn't startup.

If I change to don't check image_seq and don't return,  system will startup.

But after back-back boot/shutdown, It won't startup for ever.

I find that it died at "ADROID" logo status, and some program file can't be found.

something like that "untracked pid 7568 exited"

maybe ubi fs mount fail.

The UBI FS maybe damage to lost.

UBI: physical eraseblock size:   1048576 bytes (1024 KiB)

UBI: logical eraseblock size:    1040384 bytes

UBI: smallest flash I/O unit:    4096

UBI: VID header offset:          4096 (aligned 4096)

UBI: data offset:                8192

UBI error: process_eb: bad image sequence number 1114154050 in PEB 1281,

expected 729290202

UBI: max. sequence number:       45

any suggestion or other help?

thx

0 件の賞賛
返信
1 返信

3,459件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

I have never gotten that error (yet), but doing some search in google I found out that the error is related to a problem in the flashing of the board, that is:

1. you flash a new image incorrectly - you do not erase _whole_ flash

2. you flash a new image - by erasing only the erase blocks where you

write, but not erasing the rest of eraseblock.

That could probably be the problem. Have you tried completely erasing and reflashing the device?

0 件の賞賛
返信