UART5 getty under Ubuntu Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART5 getty under Ubuntu Linux

Jump to solution
7,234 Views
frankmiller
Contributor IV

Greetings,

I have a custom MX6 board where we've have a DB-9 serial connection on UART5.  We're running the most recent Ubuntu Linux on the system.  How can I configure the system to start a getty on that device at bootup?

Thanks,

FM

0 Kudos
Reply
1 Solution
5,287 Views
lily_zhang
NXP Employee
NXP Employee

So you hope to use UART5 as console output port. Right?

You can check the followings:

1. Ensure you have config UART5 relative pins.

2. Set early UART as UART5 if you hope to use UART5 as early console output.

uart_clk = clk_get_sys("imx-uart.4", NULL);

early_console_setup((UART5_BASE_ADDR, uart_clk);

3. Add UART5 device: imx6q_add_imx_uart(4, NULL).  If you have UART platform data, you should set accordingly. I saw your early mx6_sabresd_uart4_data __initconst is wrong. Because you mention you don't have RTS/CTS, but you enable it into the flags.

4. Then you can change your console output as UART5 into command line when you boot: console=ttymxc4.

5. For getty, you can check etc/init. If you don't want to modify getty, another method -  you can change  as       imx6q_imx_uart_data_entry(0, 5) in arch/arm/plat-mxc/devices/platform-imx-uart.c. Then use 0 for UART5 in other step 3 and 4.

View solution in original post

0 Kudos
Reply
7 Replies
5,287 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please read the document BSP_Porting_Guide_L3.0.35_1.1.0.pdf. ( Chapter 3 -- Registering a New UART Driver )  for the details.  You can download the Linux BSP document bundle from here: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

0 Kudos
Reply
5,287 Views
frankmiller
Contributor IV

Hi Jimmy,

Thanks for the reply.  I've done all of this and incorporated some other advice that was given to me on another thread.  So I have the following changes in board-mx6q_sabresd.c:

// <added>

static const struct imxuart_platform_data

  mx6_sabresd_uart4_data __initconst = {

  .flags = IMXUART_HAVE_RTSCTS | IMXUART_SDMA,

  .dma_req_rx = MX6Q_DMA_REQ_UART5_RX,

  .dma_req_tx = MX6Q_DMA_REQ_UART5_TX,

};

// </added>

static inline void mx6q_sabresd_init_uart(void)

{

        imx6q_add_imx_uart(0, NULL);

//      imx6q_add_imx_uart(2, NULL);

        imx6q_add_imx_uart(4, &mx6_sabresd_uart4_data);

//      imx6q_add_imx_uart(4, NULL);

//      imx6q_add_imx_uart(0, NULL);

}

This is the output I get when I try to boot this.  For some reason it doesnt appear to be applying these parameters to UART5.  The kernel boot hangs at this point as well.  Any thoughts?

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

imx-uart.1: ttymxc1 at MMIO 0x2184200 (irq = 2) is a IMX


0 Kudos
Reply
5,286 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to the Linux BSP reference manual (Linux_6DQ_RM_L3.0.35_1.1.0.pdf) Chapter 38 -- UART driver, there is a note (attach below) that DMA may be abnormal if not enable RTS/CTS. So please try to enable RTS/CTS.

NOTE :

If you want to use the DMA support for UART please also enable the RTS/CTS for it. The DMA may be abnormal if you do not enable the RTS/CTS.


0 Kudos
Reply
5,287 Views
frankmiller
Contributor IV

In addition to the changes you mentioned, I've found I need to do the following changes as well.  First in linux/arch/arm/plat-mxc/include/mach/mx6.h:

// <added>

#define MX6Q_UART5_BASE_ADDR            0x021f4000

// </added>

I also had to add an entry in the ..._uart_data[] table for UART5 in linux/arch/arm/plat-mxc/devices/platform-imx-usrt.c:

#ifdef CONFIG_SOC_IMX6Q

const struct imx_imx_uart_1irq_data imx6q_imx_uart_data[] __initconst = {

#define imx6q_imx_uart_data_entry(_id, _hwid)                           \

        imx_imx_uart_1irq_data_entry(MX6Q, _id, _hwid, SZ_4K)

        imx6q_imx_uart_data_entry(0, 1),

        imx6q_imx_uart_data_entry(1, 2),

        imx6q_imx_uart_data_entry(2, 3),

        imx6q_imx_uart_data_entry(3, 4),

// <added>

        imx6q_imx_uart_data_entry(4, 5),

// </added>

};

#endif /* ifdef CONFIG_SOC_IMX6Q */

These two changes allow the kernel to boot but when I look at the kernel output I get this:


imx-uart.0: ttymxc0 at MMIO 0x20200000 (irq = 58) is a IMX

imx-uart: probe of imx-uart.4 failed with error -2


Any thoughts on this error code?


Thanks,

FM


0 Kudos
Reply
5,288 Views
lily_zhang
NXP Employee
NXP Employee

So you hope to use UART5 as console output port. Right?

You can check the followings:

1. Ensure you have config UART5 relative pins.

2. Set early UART as UART5 if you hope to use UART5 as early console output.

uart_clk = clk_get_sys("imx-uart.4", NULL);

early_console_setup((UART5_BASE_ADDR, uart_clk);

3. Add UART5 device: imx6q_add_imx_uart(4, NULL).  If you have UART platform data, you should set accordingly. I saw your early mx6_sabresd_uart4_data __initconst is wrong. Because you mention you don't have RTS/CTS, but you enable it into the flags.

4. Then you can change your console output as UART5 into command line when you boot: console=ttymxc4.

5. For getty, you can check etc/init. If you don't want to modify getty, another method -  you can change  as       imx6q_imx_uart_data_entry(0, 5) in arch/arm/plat-mxc/devices/platform-imx-uart.c. Then use 0 for UART5 in other step 3 and 4.

0 Kudos
Reply
5,287 Views
frankmiller
Contributor IV

This is the code I had to add to make this work but it is finally working!

diff board-mx6q_sabresd.h board-mx6q_sabresd.h.bak

44,46c44,45

< //    MX6Q_PAD_KEY_COL1__ECSPI1_MISO,

< //    MX6Q_PAD_KEY_ROW1__GPIO_4_9,

<

---

>     MX6Q_PAD_KEY_COL1__ECSPI1_MISO,

>     MX6Q_PAD_KEY_ROW1__GPIO_4_9,

182,191c181,182

< //    MX6Q_PAD_EIM_D24__UART3_TXD,

< //    MX6Q_PAD_EIM_D25__UART3_RXD,

<

< // <added>

<     /* UART5 for external serial port */

<     MX6Q_PAD_KEY_COL1__UART5_TXD,

<     MX6Q_PAD_KEY_ROW1__UART5_RXD,

<     MX6Q_PAD_KEY_COL4__UART5_RTS,

<     MX6Q_PAD_KEY_ROW4__UART5_CTS,

< // </added>

---

>     MX6Q_PAD_EIM_D24__UART3_TXD,

>     MX6Q_PAD_EIM_D25__UART3_RXD,

225,228c216,219

<     //MX6Q_PAD_SD3_DAT4__USDHC3_DAT4_50MHZ,

<     //MX6Q_PAD_SD3_DAT5__USDHC3_DAT5_50MHZ,

<     //MX6Q_PAD_SD3_DAT6__USDHC3_DAT6_50MHZ,

<     //MX6Q_PAD_SD3_DAT7__USDHC3_DAT7_50MHZ,

---

>     MX6Q_PAD_SD3_DAT4__USDHC3_DAT4_50MHZ,

>     MX6Q_PAD_SD3_DAT5__USDHC3_DAT5_50MHZ,

>     MX6Q_PAD_SD3_DAT6__USDHC3_DAT6_50MHZ,

>     MX6Q_PAD_SD3_DAT7__USDHC3_DAT7_50MHZ,

265c256

< //    MX6Q_PAD_KEY_COL4__GPIO_4_14, /* PCIE_DIS */

---

>     MX6Q_PAD_KEY_COL4__GPIO_4_14, /* PCIE_DIS */

diff board-mx6q_sabresd.c board-mx6q_sabresd.c.bak

249a249

>     imx6q_add_imx_uart(2, NULL);

251d250

< //    imx6q_add_imx_uart(2, NULL);

1919,1923c1918,1919

< //    uart_clk = clk_get_sys("imx-uart.0", NULL);

<     uart_clk = clk_get_sys("imx-uart.4", NULL);

<

< //    early_console_setup(UART1_BASE_ADDR, uart_clk);

<     early_console_setup(UART5_BASE_ADDR, uart_clk);

---

>     uart_clk = clk_get_sys("imx-uart.0", NULL);

>     early_console_setup(UART1_BASE_ADDR, uart_clk);

diff platform-imx-uart.c platform-imx-uart.c.bak

133,139c133,136

<

< //    imx6q_imx_uart_data_entry(0, 1),

<     imx6q_imx_uart_data_entry(0, 5),

<

< //    imx6q_imx_uart_data_entry(1, 2),

< //    imx6q_imx_uart_data_entry(2, 3),

< //    imx6q_imx_uart_data_entry(3, 4),

---

>     imx6q_imx_uart_data_entry(0, 1),

>     imx6q_imx_uart_data_entry(1, 2),

>     imx6q_imx_uart_data_entry(2, 3),

>     imx6q_imx_uart_data_entry(3, 4),

diff mx6.h mx6.h.bak

286,290d285

<

< // <added>

< #define MX6Q_UART5_BASE_ADDR        0x021f4000

< // </added>

<

494,498d488

<

< // <added>

< #define MX6Q_INT_UART5            MXC_INT_UART5_ANDED

< // </added>

<




0 Kudos
Reply
5,287 Views
frankmiller
Contributor IV

I've seen this note.  Is there anyway to bring up a UART without RTS/CTS?  UART1 on this board has only the TX/RX lines connected.  I'm getting a login prompt on that port but cannot input anything to it from minicom on a Linux laptop.

Thanks,

FM

0 Kudos
Reply