UART3 can't work in 3.5.7 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART3 can't work in 3.5.7 kernel

2,874件の閲覧回数
kenwu
Contributor I


Hi

I need to use uart3 for my bluetooth module, by default, I can't find /dev/ttymxc2 when system boot up, after look into 3.5.7 kernel and modify device tree structure at ~/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi and ~/arch/arm/boot/dts/imx6q.dtsi, now I have /dev/ttymxc2.

But unfortunately, it can't work.

I want to know if I still miss any modificatioin to enable this UART3, please help, thanks.

PS. my platform is i.MX6 base board with SABRE for automotive infotainment cpu board, uart3 interface is on i.MX6 base board

Thanks in advanced

Ken

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,619件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Ken,

Can you notify this in the meta-freescale mailing list?

https://lists.yoctoproject.org/listinfo/meta-freescale

Best Regards,

Alejandro

0 件の賞賛
返信

2,619件の閲覧回数
kenwu
Contributor I

Hi

Yes, I can see that, will register now.

Ken

0 件の賞賛
返信

2,619件の閲覧回数
LeonardoSandova
Specialist I

Ken, have you tried the same setup on 3.10.17?

0 件の賞賛
返信

2,619件の閲覧回数
kenwu
Contributor I

Hi

I am sure that 3.10.9 works fine with UART3 (/dev/ttymxc2), we don’t try on 3.10.17.

In this release, it don’t provide 3.10.17.bb.

Ken

0 件の賞賛
返信