UART232/485

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART232/485

2,970 次查看
raje_embd13
Contributor I

#

Hi ,

I am working on IMX6 dual.

In our Hardware the processor GPIO's are mapped to UART(LTC28xx). The Ltc28xx working in both  RS232/RS485. On my environment  RS485 mode is controlled by Processor GPIO pins.

The dtsi file is declared as below.

The Question is:: How to use these GPIO's in UART driver at run time to check pin status and control GPIO pins ?

 &uart1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_tcs_uart1>;
 status = "okay";
 uart1_sel {
 pins = "GPIO3_IO29"; /* RS232_485_SEL */
 output-enable;
 output-low;
 };
 uart1_en {
 pins = "GPIO2_IO10"; /* RS232_485_EN */
 output-enable;
 output-high;
 };
 uart1_speed {
 pins = "GPIO3_IO20"; /* RS232_SPEED, 1 - 1 mbps, 0 - 250 kbps */
 output-enable;
 output-high;
 };
 };

pinctrl_XXX_uart1: XXX-uart1 {
 fsl,pins = <
 MX6QDL_PAD_CSI0_DAT10__UART1_TX_DATA 0x1b0b1
 MX6QDL_PAD_CSI0_DAT11__UART1_RX_DATA 0x1b0b1
 MX6QDL_PAD_EIM_D29__GPIO3_IO29 0x1b0b1
 MX6QDL_PAD_EIM_D20__GPIO3_IO20 0x1b0b1

Thanks,

Prasad

#

标签 (1)
标记 (3)
0 项奖励
回复
4 回复数

2,868 次查看
raje_embd13
Contributor I

Hi Igor,

Is this patch help's me : http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

Thanks,

RajendraPrasad

0 项奖励
回复

2,868 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rajendra

yes it may help for rs485.

Best regards
igor

0 项奖励
回复

2,868 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  VenkataNagaRajendra

for run time control of gpios, seems it is necessary to write custom

application using LTC28xx driver, which would control these gpios.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,868 次查看
raje_embd13
Contributor I

Hi Igor,

Yes, that's right. But where I can change / add  Or implement application . I need these guide lines

Thanks,

Rajendra

0 项奖励
回复