UART Recieving Problem, IMX6Q ,SDK_Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART Recieving Problem, IMX6Q ,SDK_Platform

4,502件の閲覧回数
khaledali
Contributor III

hi all,
i'm trying to run the i2c_test code imx6_sdk_platform but there is a problem in sending a character from my PC to UDOO board via uart to
choose which device
i want or exit the program
the i2c_test code locates at /sdk/driver/i2c/test

this is the segment of code that i'm trying to execute :

   do {

        printf("\n  1 - to perform a test with the i.MX6 as a master accessing an EEPROM.\n");

        printf("  2 - to perform a test with the i.MX6 as a slave device.\n");

        printf("  x - to exit.\n\n");

        do {

            sel = uart_getchar(g_debug_uart_port);

        } while (sel == NONE_CHAR);

        if (sel == 'x') {

            printf("\nTest exit.\n");

            break;

        }

        if (sel == '1')

            i2c_eeprom_at24cxx_test();

        if (sel == '2')

            i2c_imx6_slave_test();

    } while(1);

//-----------------------------------------------------------------------------------------------------------------------

my program hangs at the inner do -while loop

do {

            sel = uart_getchar(g_debug_uart_port);

        } while (sel == NONE_CHAR);

i tried to send a character from minicom and putty and the same problem appears there is no action !!!!

タグ(3)
0 件の賞賛
返信
8 返答(返信)

4,278件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi Khaled,

Otherwise can you try manually,

1) Set the baudrate

     => stty -F /dev/ttymxc(UART no) 115200

2) If you want to send data

     =>  echo  "ARAVINTH" > /dev/ttymxc(UART no)

3) If you want Receive Data

     => cat /dev/ttymxc(UART no)

Regards,

Aravinth

0 件の賞賛
返信

4,278件の閲覧回数
khaledali
Contributor III

Hi aravinthkumar,

First thank u for your kind reply
I tried this trial 2 weeks ago and i couldn't send
let me ask u did you work with SDK v1.1 ?

0 件の賞賛
返信

4,277件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi Khaled,

I'm not worked on SDK v1.1.

But i think UART same for all.

Regards,

Aravinth

0 件の賞賛
返信

4,278件の閲覧回数
khaledali
Contributor III

Hi Aravinth,
So can you send me your UART driver what ever working with SDK or something else ?
and thank u in advance

Regrards,
Khaled

0 件の賞賛
返信

4,277件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi,

In all kernel check inside below location:

driver/tty/

Regards,

Aravinth

0 件の賞賛
返信

4,277件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Khaled

after hang one can try to attach jtag and check uart regsiters, in particular

UARTx_URXD for errors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,277件の閲覧回数
khaledali
Contributor III

Hi igorpadykov,
What if i haven't a jtag ?
i'm in need of SDK v1.1 support can you help me with this ?

0 件の賞賛
返信

4,277件の閲覧回数
khaledali
Contributor III

What if i haven't a jtag to check the registers ?

0 件の賞賛
返信