UART Receiver Register (UARTx_URXD) issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART Receiver Register (UARTx_URXD) issue

1,869 Views
alielseddeek
Contributor II

Dear All,

I am trying to communicate with iMX6 quad through UART. I succeeded in establishing the transmitting part but I can't receive anything. UARTx_UTXD doesn't respond in any way whether I press any key or not.

I tried also to follow the steps mentioned in section 64.13.1 "Programming the UART in RS-232 mode" but I had the same issue. All the previous experiments were done baremetal through the SDK.

Did I miss something regarding the configuration settings or something?!

Thanks in Advance

Best regards
Ali Elseddeek

Labels (1)
3 Replies

1,784 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ali

please look at attached example from sdk and description

in Chapter 33 Configuring the UART Driver pdf file.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,784 Views
alielseddeek
Contributor II

Thanks Igor for your reply. I already have seen this chapter in addition to attached example but I had no clue. I also would like to mention that the example receiver part doesn't work either.

Question1) Is there any configuration that is specific for the receiving part since I can transmit anything I want?
Question2) Note that I am using Uart2 module in my tests so is there a possibility that I should use another one?

Thanks in advance

Best regards
Ali Elseddeek

0 Kudos
Reply

1,784 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ali

suggest to look at attached one more example.

Best regards
igor

0 Kudos
Reply