UART RX SDMA problem on iMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART RX SDMA problem on iMX6Q

ソリューションへジャンプ
5,907件の閲覧回数
AlexeyT
Contributor III

Hi All,

I am facing a quite a strange issue with the subject.

It look like it only partially works.

I have UART4 configured for SDMA with

- RXTL set to 16 bytes

- TXTL set to 16 bytes

- DMA ageing turned on

- SDMA watermark level set to 16 bytes as well

I am having problem when transfer size is exactly 16 bytes, in this case SDMA interrupt does not trigger.

If I send from 1 to 15 bytes I receive RX interrupt and get the data correctly.

If I send 16 bytes I don't get RX interrupt at all.

If I send 16 bytes and then 1 extra byte after a delay I will get interrupt and read all 17 bytes ok.

To me it look like I can get DMA data ageing interrupt but can't get normal watermark based interrupt.

I tripple checked UART code and cannot find any issue, everything look completely fine.

Checked SDMA channel configuration and found no configuration error as well.

Can you please suggest where do I need to have a look to check fo SDMA possible watermark errors?

It look like only UART that suffers, other devices which use SDMA work completely fine.

My platform is Windows Embedded Compact 7.

Thanks,

Alexey

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
4,865件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

When DMA is applied, some issues may be caused by improper FIFO read

watermark level : say,  configure it so, that burst length is half of FIFO. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,865件の閲覧回数
shinichiichimur
Contributor I

dear yuri,

I see, I'm ok. thanks.

Regard,

Ichimura

0 件の賞賛
返信
4,865件の閲覧回数
shinichiichimur
Contributor I

Dear Yuri,

I have the similar issue on iMX6SoloLite, and I can't fix it with Alexey's way. I configured below, 

- TXTL set to 16 bytes

- TXTL set to 16 bytes

- DMA ageing turned on

- SDMA watermark level set to 8 bytes as well

but SDMA interrupt didn't trigger with exact 16 bytes. Does this solution work on iMX6SoloLite?

 

BR,

Ichimura

0 件の賞賛
返信
4,865件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello, Ichimura !

  Is it possible for You to create separate thread in this Community or

create request Sales and Support|NXP   ? 

Regards,

Yuri.

0 件の賞賛
返信
4,866件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

When DMA is applied, some issues may be caused by improper FIFO read

watermark level : say,  configure it so, that burst length is half of FIFO. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,865件の閲覧回数
AlexeyT
Contributor III

Hi Yuri,

I reduced watermark level in SDMA configuration to 8 bytes which is 1/2 of RXTL (keeping RXTL at 16 bytes).

It fixed the issue.

Tried other configuration variants but nothing else seem to work.

Thanks for help.

Alexey

0 件の賞賛
返信