UART Debug port number in IMX7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART Debug port number in IMX7

1,685件の閲覧回数
logeshs
Contributor II

Hi,

Kindly help me, which UART port is used for debugging in IMX7 (Part number # MCIMX7D7DVK10SC)

Thanks & Regards,

Logesh

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,476件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 On iMX7DSABRESD board J11 connector is used for Debug UART (via USB).

According to board schematic: Debug UART1 is intended for Cortex-A7;

Debug UART2 for Cortex-M4.

   NXP BSP(s) uses such approach, but customers can use any available UART ports

(and pins) for their applications, assuming BSP modification, if needed. 

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,476件の閲覧回数
logeshs
Contributor II

Also Kindly suggest shall we use any of below UART ports for debugging,

1. UART1 (Pin# D16 & D7)

2. UART2 (Pin# G28 & D20)

If we are not able to use the above ports for debugging kindly request you to provide correct the UART port ID with pin numbers.

Thanks & Regards

Logesh

0 件の賞賛
返信