Using NXP Android automotive 12.1 found an UAF in V4l2Dev
soc: imx8qm
linux 5.15.52
NXP's android automotive 12.1
#0 std::__1::__vector_base<unsigned int, std::__1::allocator<unsigned int> >::~__vector_base() in external/libcxx/include/vector:462:9
-> std::__1::vector<unsigned int, std::__1::allocator<unsigned int> >::~vector() in external/libcxx/include/vector:556:5
-> android::V4l2Dev::~V4l2Dev() in vendor/nxp/imx_android_mm/codec2/v4l2_dev/V4l2Dev.h:69:7
-> android::IsiFilter::onRelease() in vendor/nxp/imx_android_mm/codec2/filter/isi/IsiFilter.cpp:163:9
#1 android::IsiFilter::~IsiFilter() in vendor/nxp/imx_android_mm/codec2/filter/isi/IsiFilter.cpp:56:5
#2 android::IsiFilter::~IsiFilter() in vendor/nxp/imx_android_mm/codec2/filter/isi/IsiFilter.cpp:54:24
#3 std::__1::__function::__value_func<void (C2Component*)>::operator()(C2Component*&&) const in external/libcxx/include/functional:1799:16
-> std::__1::function<void (C2Component*)>::operator()(C2Component*) const in external/libcxx/include/functional:2347:12
-> android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0::operator()(C2Component*) in vendor/nxp/imx_android_mm/codec2/store/ImxC2Store.cpp:421:17
-> decltype(std::__1::forward<android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0&>(fp)(std::__1::forward<C2Component*>(fp0))) std::__1::__invoke<android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0&, C2Component*>(android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0&, C2Component*&&) in external/libcxx/include/type_traits:4353:1
-> void std::__1::__invoke_void_return_wrapper<void>::__call<android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0&, C2Component*>(android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0&, C2Component*&&) in external/libcxx/include/__functional_base:349:9
-> std::__1::__function::__alloc_func<android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0, std::__1::allocator<android::ImxC2Store::ComponentBox::createComponent(unsigned int, std::__1::shared_ptr<C2Component>*, std::__1::function<void (C2Component*)>)::$_0>, void (C2Component*)>::operator()(C2Component*&&) in external/libcxx/include/functional:1527:16
-> std::__1::__function::__func<android::ImxC2Store::ComponentBox::createInterface(unsigned int, std::__1::shared_ptr<C2ComponentInterface>*, std::__1::function<void (C2ComponentInterface*)>)::$_1, std::__1::allocator<android::ImxC2Store::ComponentBox::createInterface(unsigned int, std::__1::shared_ptr<C2ComponentInterface>*, std::__1::function<void (C2ComponentInterface*)>)::$_1>, void (C2ComponentInterface*)>::operator()(C2ComponentInterface*&&) in external/libcxx/include/functional:1651:12
#4 std::__1::__function::__value_func<void (C2Component*)>::operator()(C2Component*&&) const in external/libcxx/include/functional:1799:16
-> std::__1::function<void (C2Component*)>::operator()(C2Component*) const in external/libcxx/include/functional:2347:12
-> std::__1::__shared_ptr_pointer<android::IsiFilter*, std::__1::function<void (C2Component*)>, std::__1::allocator<android::IsiFilter> >::__on_zero_shared() in external/libcxx/include/memory:3640:5
#5 std::__1::__shared_count::__release_shared() in external/libcxx/include/memory:3544:9
-> std::__1::__shared_weak_count::__release_shared() in external/libcxx/include/memory:3586:27
-> std::__1::shared_ptr<C2Component>::~shared_ptr() in external/libcxx/include/memory:4522:19
-> android::FilterWrapper::Component::~Component() in frameworks/av/media/codec2/hidl/plugin/internal/FilterWrapper.h:52:12
#6 std::__1::allocator<android::FilterWrapper::Component>::destroy(android::FilterWrapper::Component*) in external/libcxx/include/memory:1881:64
-> void std::__1::allocator_traits<std::__1::allocator<android::FilterWrapper::Component> >::__destroy<android::FilterWrapper::Component>(std::__1::integral_constant<bool, true>, std::__1::allocator<android::FilterWrapper::Component>&, android::FilterWrapper::Component*) in external/libcxx/include/memory:1743:18
-> void std::__1::allocator_traits<std::__1::allocator<android::FilterWrapper::Component> >::destroy<android::FilterWrapper::Component>(std::__1::allocator<android::FilterWrapper::Component>&, android::FilterWrapper::Component*) in external/libcxx/include/memory:1596:14
-> std::__1::__vector_base<android::FilterWrapper::Component, std::__1::allocator<android::FilterWrapper::Component> >::__destruct_at_end(android::FilterWrapper::Component*) in external/libcxx/include/vector:427:9
-> std::__1::__vector_base<android::FilterWrapper::Component, std::__1::allocator<android::FilterWrapper::Component> >::clear() in external/libcxx/include/vector:370:29
-> std::__1::__vector_base<android::FilterWrapper::Component, std::__1::allocator<android::FilterWrapper::Component> >::~__vector_base() in external/libcxx/include/vector:464:9
-> std::__1::vector<android::FilterWrapper::Component, std::__1::allocator<android::FilterWrapper::Component> >::~vector() in external/libcxx/include/vector:556:5
-> android::(anonymous namespace)::WrappedEncoderInterface::~WrappedEncoderInterface() in frameworks/av/media/codec2/hidl/plugin/FilterWrapper.cpp:817:49
#7 std::__1::__shared_count::__release_shared() in external/libcxx/include/memory:3544:9
-> std::__1::__shared_weak_count::__release_shared() in external/libcxx/include/memory:3586:27
-> std::__1::shared_ptr<C2ComponentInterface>::~shared_ptr() in external/libcxx/include/memory:4522:19
-> android::hardware::media::c2::V1_0::utils::(anonymous namespace)::CompIntf::~CompIntf() in frameworks/av/media/codec2/hidl/1.0/utils/ComponentInterface.cpp:47:8
-> android::hardware::media::c2::V1_0::utils::(anonymous namespace)::CompIntf::~CompIntf() in frameworks/av/media/codec2/hidl/1.0/utils/ComponentInterface.cpp:47:8
#8 std::__1::default_delete<android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf>::operator()(android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf*) const in external/libcxx/include/memory:2339:5
-> std::__1::unique_ptr<android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf, std::__1::default_delete<android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf> >::reset(android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf*) in external/libcxx/include/memory:2652:7
-> std::__1::unique_ptr<android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf, std::__1::default_delete<android::hardware::media::c2::V1_0::utils::ConfigurableC2Intf> >::~unique_ptr() in external/libcxx/include/memory:2606:19
-> android::hardware::media::c2::V1_0::utils::CachedConfigurable::~CachedConfigurable() in frameworks/av/media/codec2/hidl/1.0/utils/include/codec2/hidl/1.0/Configurable.h:105:8
-> android::hardware::media::c2::V1_0::utils::CachedConfigurable::~CachedConfigurable() in frameworks/av/media/codec2/hidl/1.0/utils/include/codec2/hidl/1.0/Configurable.h:105:8
-> android::hardware::media::c2::V1_0::utils::CachedConfigurable::~CachedConfigurable() in frameworks/av/media/codec2/hidl/1.0/utils/include/codec2/hidl/1.0/Configurable.h:105:8
-> virtual thunk to android::hardware::media::c2::V1_0::utils::CachedConfigurable::~CachedConfigurable() in frameworks/av/media/codec2/hidl/1.0/utils/include/codec2/hidl/1.0/Configurable.h:0:0
#9 android::RefBase::decStrong(void const*) const in system/core/libutils/RefBase.cpp:475:13
#10 android::sp<android::hidl::base::V1_0::IBase>::~sp() in system/core/libutils/include/utils/StrongPointer.h:305:16
-> android::hidl::base::V1_0::BnHwBase::~BnHwBase() in out/soong/.intermediates/system/libhidl/transport/base/1.0/android.hidl.base@1.0_genc++/gen/android/hidl/base/1.0/BaseAll.cpp:750:1
#11 android::hardware::media::c2::V1_0::BnHwConfigurable::~BnHwConfigurable() in out/soong/.intermediates/hardware/interfaces/media/c2/1.0/android.hardware.media.c2@1.0_genc++/gen/android/hardware/media/c2/1.0/ConfigurableAll.cpp:839:1
#12 android::hardware::media::c2::V1_0::BnHwConfigurable::~BnHwConfigurable() in out/soong/.intermediates/hardware/interfaces/media/c2/1.0/android.hardware.media.c2@1.0_genc++/gen/android/hardware/media/c2/1.0/ConfigurableAll.cpp:837:39
-> android::hardware::media::c2::V1_0::BnHwConfigurable::~BnHwConfigurable() in out/soong/.intermediates/hardware/interfaces/media/c2/1.0/android.hardware.media.c2@1.0_genc++/gen/android/hardware/media/c2/1.0/ConfigurableAll.cpp:837:39
-> virtual thunk to android::hardware::media::c2::V1_0::BnHwConfigurable::~BnHwConfigurable() in out/soong/.intermediates/hardware/interfaces/media/c2/1.0/android.hardware.media.c2@1.0_genc++/gen/android/hardware/media/c2/1.0/ConfigurableAll.cpp:0:0
#13 android::RefBase::decStrong(void const*) const in system/core/libutils/RefBase.cpp:475:13
#14 android::hardware::IPCThreadState::processPendingDerefs() in system/libhwbinder/IPCThreadState.cpp:510:22
-> android::hardware::IPCThreadState::joinThreadPool(bool) in system/libhwbinder/IPCThreadState.cpp:546:9
#15 android::hardware::PoolThread::threadLoop() in system/libhwbinder/ProcessState.cpp:61:33
#16 android::Thread::_threadLoop(void*) in system/core/libutils/Threads.cpp:759:32
#17 thread_data_t::trampoline(thread_data_t const*) in system/core/libutils/Threads.cpp:99:16
#18 __pthread_start(void*) in bionic/libc/bionic/pthread_create.cpp:364:18
#19 __start_thread in bionic/libc/bionic/clone.cpp:53:16Fix:
diff --git a/codec2/filter/isi/IsiFilter.cpp b/codec2/filter/isi/IsiFilter.cpp
index 909afab..a99a933 100644
--- a/codec2/filter/isi/IsiFilter.cpp
+++ b/codec2/filter/isi/IsiFilter.cpp
@@ -47,7 +47,9 @@ static const uint32_t destination_format_table[]={
IsiFilter::IsiFilter(c2_node_id_t id, C2String name, const std::shared_ptr<C2ReflectorHelper>& helper, const std::shared_ptr<IsiFilterInterface> &intfImpl)
: IMXC2ComponentBase(std::make_shared<IMXInterface<IsiFilterInterface>>(name, id, intfImpl)),
- mIntfImpl(intfImpl)
+ mIntfImpl(intfImpl),
+ mFd(-1),
+ mDev(nullptr)
{
(void)helper;
}
diff --git a/codec2/filter/isi/IsiFilter.h b/codec2/filter/isi/IsiFilter.h
index 4f72357..ea2edcc 100644
--- a/codec2/filter/isi/IsiFilter.h
+++ b/codec2/filter/isi/IsiFilter.h
@@ -21,6 +21,8 @@ namespace android {
class IsiFilter : public IMXC2ComponentBase{
public:
explicit IsiFilter(c2_node_id_t id, C2String name, const std::shared_ptr<C2ReflectorHelper>& helper, const std::shared_ptr<IsiFilterInterface> &intfImpl);
+ IsiFilter(const IsiFilter&) = delete;
+ IsiFilter& operator=(const IsiFilter&) = delete;
virtual ~IsiFilter();