U-boot-imx upgrade

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot-imx upgrade

1,915件の閲覧回数
MJaroc
Contributor II

Hi,

i need to upgrade u-boot in working device. I cant use UUU or upgrade from tftp in u-boot console - it must be posible in working linux console. I now the risk. Ill try to unlock write mmcblk2boot0 and dd u-boot.bin file to /dev/mmcblk2boot0, but after that system is not booting. DNF only upgrade binarry file in /boot/ directory, it doesnt affect to bootloader.

Can anyone help me with this? For now i can only UUU u-boot.

Working system:
Linux visionsom-8mm-cb-std 5.4.24-lts-somlabs_imx_5.4.24_2.1.0+gd0ce74ff14da #1 SMP PREEMPT Fri Feb 24 11:59:09 UTC 2023 aarch64 aarch64 aarch64 GNU/Linux

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,871件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If You want to upgrade uboot there is not other option than erase and burn with new uboot, you are trying to erase so the uboot is gone, but you have to erase and burn uboot.

Regards

0 件の賞賛
返信

1,868件の閲覧回数
MJaroc
Contributor II

Hi,

i erase uboot from mmcblk2boot0 and program (by "dd" program) with u-boot.bin from YOCTO compilation, but system doesnt boot. I succesfully erase bootloader and i ask how to program a new one (maybe i need to write to specific addres or i burn a wrong file).

0 件の賞賛
返信

1,851件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Read the documentation of the board, probably you need modify sw, before and after burn the SD image.

Regards

 

0 件の賞賛
返信