U-boot flashing using JTAG on iMX8MQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

U-boot flashing using JTAG on iMX8MQ

1,555 次查看
nirmalluhana
Contributor IV

Hi,

I am working on iMX8MQ based custom board.

How to I flash u-boot using JTAG interface?

For that which JTAG emulator I can use?

If there is any steps or guide available to do the same is really helpful.

Best regards,

Nirmal

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,420 次查看
igorpadykov
NXP Employee
NXP Employee

Hi NIRMAL

unfortunately uboot flashing with jtag is not supported in nxp bsps,

one can try to reproduce with jtag uuu (using its sources) flashing steps:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复