U-boot flashing using JTAG on iMX8MQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot flashing using JTAG on iMX8MQ

1,575件の閲覧回数
nirmalluhana
Contributor IV

Hi,

I am working on iMX8MQ based custom board.

How to I flash u-boot using JTAG interface?

For that which JTAG emulator I can use?

If there is any steps or guide available to do the same is really helpful.

Best regards,

Nirmal

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,440件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi NIRMAL

unfortunately uboot flashing with jtag is not supported in nxp bsps,

one can try to reproduce with jtag uuu (using its sources) flashing steps:

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信