U-boot flash in NAND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

U-boot flash in NAND

2,095 次查看
hajimohammed
Contributor III

Hi,

 Am using Linux-3.14.38 kernel, i wanted to flash u-boot.imx file to NAND using linux command. When flashing from MFG tool, it's working fine and doing it manually using the below commands to NAND. It flashes successfully to the NAND, when boot its not booting

$ flash_erase /dev/mtd0 0 0

$ kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 u-boot.imx

Have taken the nanddump log for MFG tool and the manual command  NAND write.

nandump for MFG TOOL                      

0x00000000: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00000010: 00 00 00 00 00 00 6f  fb   ff   ff  46 43 42 20 00 00
0x00000020: 00 01 50 3c 19 06 00 00 00 00 00 08 00 00 40 08
0x00000030: 00 00 40 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00000040: 00 00 04 00 00 00 00 02 00 00 00 02 00 00 04 00
0x00000050: 00 00 0a 00 00 00 03 00 00 00 00 00 00 00 00 00

nanddump for Command Line:

0x00000000: 00 00 6f fb ff ff 46 43 42 20 00 00 00 01 50 3c
0x00000010: 19 06 00 00 00 00 00 08 00 04 40 08 00 00 40 00
0x00000020: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 04 00
0x00000030: 00 00 00 02 00 00 00 02 00 00 04 00 00 00 0a 00
0x00000040: 00 00 03 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00000050: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

There is difference in values when we compare both. you can see the difference in the nanddump (6f value is flashed at the 0x00000010 address while doing through MFG tool but it got flashed at 0x00000000. location when we do manually)

What could be the reason for this issue. Any suggestions will be helpful

标签 (4)
3 回复数

1,767 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please double check partitioning for the NAND :

""part_uboot=1"" -s ""part_kernel=2"" -s ""part_dtb=3"" -s ""part_rootfs=4""

Looks like for U-boot /dev/mtd1 should be used.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复

1,767 次查看
hajimohammed
Contributor III

Hi,

/dev/mtd0 is configured as U-boot partition , below are the NAND partition details 

0x000000000000-0x000000a00000 : "boot"
0x000000a00000-0x000001a00000 : "kernel"
0x000001a00000-0x000002a00000 : "dtb"
0x000002a00000-0x000010000000 : "rootfs"

0 项奖励
回复

1,767 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  You wrote "When flashing from MFG tool, it's working fine ". Please check carefully 

the ucl2.xml file - what commands and parameters are used there.

Regards,

Yuri.