U-boot config to imx8mn ddr4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

U-boot config to imx8mn ddr4

1,474 次查看
arrivederccimamasita
Contributor III

Hi Everyone!

I'm struggling with fsl-image-test compliance for the imx8mnevk development board, with the DRAM version of DDR4.

I am having trouble configuring the u-boot for this type of DRAM.

I have managed to do the uuu load thanks to the precompiled bootloader from the demo images. Even so, I would like to be able to do this configuration from the Yocto recipes, could someone give me some clarification.

I'm using kernel version 5.4.70, any roadmap to address this situation?

Thank you very much

0 项奖励
回复
3 回复数

1,434 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @arrivederccimamasita !

Please try:

mkdir imx-yocto-bsp

cd imx-yocto-bsp

repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml

repo sync

 

Now, for the configuration of DDR4:

DISTRO=fsl-imx-xwayland MACHINE=imx8mnddr4evk source imx-setup-release.sh -b linux

 

Then you will be able to build the image with bitbake, for example:

bitbake imx-image-full

 

 

I hope this can help to you.

Best regards!

0 项奖励
回复

1,419 次查看
arrivederccimamasita
Contributor III

Hi @Manuel_Salas 

Thanks for the response,

Unfortunately, I still face some problems compiling imx-boot due to bad deployment for the DDR firmware by the u-boot-imx. 

/tmp/deploy/images/imx8mnddr4evk/ddr4_imem_1d_201810.bin': No such file or directory

 

Some idea for what is going on? Is u-boot-imx not compiling any ddr_firmware at all or is only a deployment failure?

 

Thanks for the response!

 

0 项奖励
回复

1,393 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @arrivederccimamasita!

 

Is there some special to do? I would like replicate your issue?

 

What ubuntu version are you using? 

 

Best regards!

0 项奖励
回复