U-boot cannot cover by using mfgtool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot cannot cover by using mfgtool

2,235 Views
wangtsungli
Contributor IV

Hi community,

I'm working on i.MX6 Quad sabre-SD platform and build Android 6 as my image.

Here is the situation now.

On the first burning image, u-boot seems working well.

And I tried to change the u-boot environment via console and saveenv to change environment settings.

After that I tried to update image via mfgtool to cover the u-boot environment which I had changed before.

However it did not success, u-boot environment is still the same.

The strange thing is that mfgtool still show burning success to me.

Below is my ucl2.xml.

<UCL>
<CFG>
<STATE name="BootStrap" dev="MX6D" vid="15A2" pid="0061"/>
<STATE name="BootStrap" dev="MX6Q" vid="15A2" pid="0054"/>
<STATE name="Updater" dev="MSC" vid="066F" pid="37FF"/>
</CFG>
<LIST name="eMMC-Android" desc="Choose eMMC as media">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6q%plus%%board%_sd.imx" ifdev="MX6Q">Loading U-boot</CMD>
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6dl%plus%%board%_sd.imx" ifdev="MX6D">Loading U-boot</CMD>

<CMD state="BootStrap" type="load" file="firmware/zImage" address="0x12000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q MX6D">Loading Kernel.</CMD>


<CMD state="BootStrap" type="load" file="firmware/%initramfs%" address="0x12C00000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q MX6D">Loading Initramfs.</CMD>

<CMD state="BootStrap" type="load" file="firmware/zImage-imx6q-%board%%ldo%.dtb" address="0x18000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6Q">Loading device tree.</CMD>
<CMD state="BootStrap" type="load" file="firmware/zImage-imx6dl-%board%%ldo%.dtb" address="0x18000000"
loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" ifdev="MX6D">Loading device tree.</CMD>

<CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>

<!-- create partition -->
<CMD state="Updater" type="push" body="send" file="mksdcard-android%data_type%.sh.tar">Sending partition shell</CMD>
<CMD state="Updater" type="push" body="$ tar xf $FILE "> Partitioning...</CMD>
<CMD state="Updater" type="push" body="$ sh mksdcard-android%data_type%.sh /dev/mmcblk%mmc%"> Partitioning...</CMD>

<!-- burn uboot -->
<CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk%mmc% bs=1k seek=768 conv=fsync count=512">clear u-boot arg</CMD>
<CMD state="Updater" type="push" body="$ echo 0 > /sys/block/mmcblk%mmc%boot0/force_ro">access boot partition 1</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/%folder%/u-boot-imx%soc%%ldo%.imx" >Sending u-boot.bin</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk%mmc%boot0 bs=512 seek=2 ">write U-Boot to sd card</CMD>
<CMD state="Updater" type="push" body="$ echo 1 > /sys/block/mmcblk%mmc%boot0/force_ro"> re-enable read-only access </CMD>
<CMD state="Updater" type="push" body="$ sync">Sync file system</CMD>

<!-- burn kernel -->
<CMD state="Updater" type="push" body="$ mmc bootpart enable 1 1 /dev/mmcblk%mmc%">enable boot partion 1 to boot</CMD>
<CMD state="Updater" type="push" body="$ ls -l /dev/mmc* ">Formatting sd partition</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/%folder%/boot-imx%soc%%ldo%.img" >Sending and writting boot.img</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk%mmc%p1">write boot.img</CMD>

<!-- burn system -->
<CMD state="Updater" type="push" body="$ mkfs.ext4 -E nodiscard /dev/mmcblk%mmc%p5">Formatting system partition</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -E nodiscard /dev/mmcblk%mmc%p6">Formatting cache partition</CMD>
<CMD state="Updater" type="push" body="$ mkfs.ext4 -E nodiscard /dev/mmcblk%mmc%p7">Formatting device partition</CMD>
<CMD state="Updater" type="push" body="$ mount -o remount,size=1500M rootfs /">change size of tmpfs</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/%folder%/system.img" >Sending system.img</CMD>
<CMD state="Updater" type="push" body="$ simg2img $FILE /dev/mmcblk%mmc%p5">writting sparse system.img</CMD>

<!-- Write userdata.img is optional, for some customer this is needed, but it's optional. -->
<!-- Also, userdata.img will have android unit test, you can use this to do some auto test. -->
<!-- <CMD state="Updater" type="push" ="ignore" body="pipe dd of=/dev/mmcblk0p7" file="file/android/userdate.img"> Sending userdata.img(optional) </CMD>
<CMD state="Updater" type="push" body="frf">flush the memory.</CMD> -->

<!-- burn recovery -->
<CMD state="Updater" type="push" body="pipe dd of=/dev/mmcblk%mmc%p2 bs=512" file="files/android/%folder%/recovery-imx%soc%%ldo%.img">Sending and writting recovery.img</CMD>
<CMD state="Updater" type="push" body="$ sync">Sync file system</CMD>
<CMD state="Updater" type="push" body="frf">Finishing rootfs write</CMD>

<CMD state="Updater" type="push" body="$ echo Update Complete!">Done</CMD>

</LIST>

How can I solve this problem?

Please help!

 Thanks in Advanced!

0 Kudos
Reply
3 Replies

1,935 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

I quite do not understand well your question.

However, If you change the u-boot environment settings, you will not need to rerun the MFGtool if you saved the environment. The Android image will start with the new environment variables. Hope this can solve your problem.

Best Regards,

Diego.  

0 Kudos
Reply

1,935 Views
wangtsungli
Contributor IV

Hi Adrian,

First I tried to change u-boot environment from A to B.

Second I tried to change my u-boot environment back to A by using mfgtool to update whole image including system.img and boot.img  etc.

But in the second step it cannot work.

Even I tried to update whole image via mfgtool, u-boot environment is still be B not be A.

How can I fix this situation?

0 Kudos
Reply

1,935 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

If you want to go to the default environment, you can try with the below u-boot command:

u-boot -> default env -a

u-boot -> saveenv

With this command will be restored to the default environment.

Hope this can solve your problem.

Best Regards,

Diego.

0 Kudos
Reply