U-boot SPI driver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-boot SPI driver problem

ソリューションへジャンプ
3,053件の閲覧回数
kuda
Contributor II

Dear NXP community,

I am developing a custom board based on the Coral System-on-Module.

Since I want to show Splash Screen on uboot , I am trying to enable mxc_spi.c first.
There is get an error message "No cs-gpios property" when call the mxc_spi_probe api.

Is mxc_spi.c support imx8mq(Coral System-on-Module) ? or any command?

the attached is our dts & code.

                                                                                                      kuda

0 件の賞賛
返信
1 解決策
3,049件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kuda

 

seems some third party boards support uboot "cs-gpios" ecspi property as in below example:

https://github.com/boundarydevices/u-boot-imx6/blob/boundary-v2020.10/arch/arm/dts/imx8mq-nitrogen8m...

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,050件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kuda

 

seems some third party boards support uboot "cs-gpios" ecspi property as in below example:

https://github.com/boundarydevices/u-boot-imx6/blob/boundary-v2020.10/arch/arm/dts/imx8mq-nitrogen8m...

 

Best regards
igor

0 件の賞賛
返信