U-Boot releases for RIoTboard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

U-Boot releases for RIoTboard

跳至解决方案
2,956 次查看
Xavier
Contributor III

Hi! I'm currently trying to find a recent version of U-Boot for the RIoTboard. Indeed the one provided in the sources of Android on the Embest website (RIoTboard Development Platform) was released in August 2009 and it seems I'm missing some utilities (usb notably) I need to update U-Boot thanks to a USB stick. Any ideas?

标签 (4)
标记 (2)
0 项奖励
回复
1 解答
2,370 次查看
fabio_estevam
NXP Employee
NXP Employee

Xavier,

Riotboard is supported in mainline U-boot:

http://git.denx.de/?p=u-boot.git;a=blob;f=board/embest/mx6boards/mx6boards.c;h=f8c746824a7625edb6a36...

So just use the lastest 2015.01 and your Riotboard will work there ;-)

Regards,

Fabio Estevam

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,371 次查看
fabio_estevam
NXP Employee
NXP Employee

Xavier,

Riotboard is supported in mainline U-boot:

http://git.denx.de/?p=u-boot.git;a=blob;f=board/embest/mx6boards/mx6boards.c;h=f8c746824a7625edb6a36...

So just use the lastest 2015.01 and your Riotboard will work there ;-)

Regards,

Fabio Estevam

0 项奖励
回复
2,370 次查看
Xavier
Contributor III

My bad... I should've paid more attention. Sorry guys!

0 项奖励
回复
2,370 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Xavier,

I did some lookup on this on google and found that there are a couple of available BSPs here:

http://www.element14.com/community/docs/DOC-68442/l/riotboard-bsp-images-and-tools-download--android...

(check the comments section from that link)

I recommend you to ask in the RIoT board forums too, I'm not sure if they have more recent versions of u-boot.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------