U-Boot: not work output on UART2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

U-Boot: not work output on UART2

跳至解决方案
12,009 次查看
BrilliantovKiri
Senior Contributor I

Hello!

We are use UART2 on our board, follow my configuration for U-Boot.

#define CONFIG_MXC_UART
#define CONFIG_UART_BASE_ADDR   UART2_BASE_ADDR

#define CONFIG_BAUDRATE            115200
#define CONFIG_SYS_BAUDRATE_TABLE  {9600, 19200, 38400, 57600, 115200}

#define CONFIG_EXTRA_ENV_SETTINGS                                   \
            "bootargs_base=setenv bootargs console=ttymxc1,115200\0"\
            "bootargs_nand=setenv bootargs ${bootargs} ip=off " \
                    "root=/dev/mtdblock4 rootfstype=jffs2\0" \
            "bootcmd_nand=run bootargs_base bootargs_nand; " \
                    "nboot 0x80700000 0 0x1080000; bootm\0" \
            "bootargs_mmc=setenv bootargs ${bootargs} ip=off "  \
                    "root=/dev/mmcblk0p1 rootwait rw\0"         \
            "bootcmd_mmc=run bootargs_base bootargs_mmc; "      \
                    "mmc dev 0; "                               \
                    "mmc read ${loadaddr} 0x800 0x1800; bootm\0"\
            "bootcmd=run bootcmd_mmc\0"

static void setup_uart(void)

{

        u32 cfg = (PAD_CTL_HYS_ENABLE | PAD_CTL_PKE_ENABLE |

                        PAD_CTL_PUE_PULL | PAD_CTL_100K_PU |

                        PAD_CTL_ODE_OPENDRAIN_NONE | PAD_CTL_DRV_HIGH);

        /* UART2 RXD */

        mxc_request_iomux(MX53_PIN_EIM_D27, IOMUX_CONFIG_ALT2);

        mxc_iomux_set_pad(MX53_PIN_EIM_D27, cfg);

        mxc_iomux_set_input(MUX_IN_UART2_IPP_UART_RXD_MUX_SELECT_INPUT,

                        INPUT_CTL_PATH1);

        /* UART2 TXD */

        mxc_request_iomux(MX53_PIN_EIM_D26, IOMUX_CONFIG_ALT2);

        mxc_iomux_set_pad(MX53_PIN_EIM_D26, cfg);

}


Unfortunally I not get any U-Boot output if it started from NAND or SD, but I get U-Boot output and can work with it if I load it via MfgTool.

How should I configure uart for work with U-Boot?

Thank you and excuse me my bad english.

标签 (1)
标记 (2)
1 解答
7,231 次查看
BrilliantovKiri
Senior Contributor I

Ok, problem in Linux solved, in my case arch/arm/plat-mxc/include/mach/iomux-mx53.h have incorrect parameters for _MX53_PAD_EIM_D26__UART2_TXD_MUX, please see attache.

在原帖中查看解决方案

0 项奖励
回复
13 回复数
7,232 次查看
BrilliantovKiri
Senior Contributor I

Ok, problem in Linux solved, in my case arch/arm/plat-mxc/include/mach/iomux-mx53.h have incorrect parameters for _MX53_PAD_EIM_D26__UART2_TXD_MUX, please see attache.

0 项奖励
回复
7,231 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Kirill,

       From your description, u-boot in OS Firmware can normally work in memory,and startup messages can output to console when MFG Tool is burning images.So your configuration for UART2 in u-boot is correct.

       After burning images, when you normally boot system form SD card, you can't see startup messages on console, I judge ROM code didn't normally read u-boot code into iRAM or read unexpected code.

       So I think you should check u-boot, the issue should be from u-boot. Could you tell me which BSP version you are using ?

Regards,

Weidong

0 项奖励
回复
7,231 次查看
BrilliantovKiri
Senior Contributor I

Hello, Weidong!

How can I check U-Boot, what parameters should I recheck?

Now I work with U-Boot 2009.08 and Linux-2.6.35.3 form L2.6.35_11.09.01_ER_source_bundle.tar.gz

>

0 项奖励
回复
7,231 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Kirill,

      Wait, Let us confirm boot mode setting on your board at first, Assume you boot from eSDHC3 port with SD card.

(1)BOOT_MODE0=0 & BOOT_MODE1=1

(2)EIM PADs setting

EIM_A20 = 1

EIM_A19 = 0

EIM_A18 = 1

EIM_EB0 = 0

EIM_EB1 = 1

EIM_DA0 = 0

---------------------

EIM_DA6/EIM_A21/EIM_LBA/EIM_DA1/EIMDA2 = 1

--------------------

EIM_A22/EIM_A16/EIM_DA7/EIM_DA8 = 0

Then how about your settings ? The boot settings can also cause boot failure !

Regards,

Weidong

0 项奖励
回复
7,231 次查看
BrilliantovKiri
Senior Contributor I

Hello, Weidong!

I use eSDHC1 for booting.

My configuration for booting from SD:

#define CONFIG_CMD_MMC

#ifdef CONFIG_CMD_MMC

        #define CONFIG_MMC                      1

        #define CONFIG_GENERIC_MMC

        #define CONFIG_IMX_MMC

        #define CONFIG_SYS_FSL_ESDHC_NUM        1

        #define CONFIG_SYS_FSL_ESDHC_ADDR       0

        #define CONFIG_SYS_MMC_ENV_DEV  0

        #define CONFIG_DOS_PARTITION    1

        #define CONFIG_CMD_FAT          1

        #define CONFIG_CMD_EXT2         1

        /* detect whether ESDHC1 or ESDHC3 is boot device */

        #define CONFIG_DYNAMIC_MMC_DEVNO

        #define CONFIG_EMMC_DDR_PORT_DETECT

        #define CONFIG_EMMC_DDR_MODE

        /* port 1 (ESDHC3) is 8 bit */

        #define CONFIG_MMC_8BIT_PORTS   0x2

#endif

#ifdef CONFIG_CMD_MMC

struct fsl_esdhc_cfg esdhc_cfg[2] = {

        {MMC_SDHC1_BASE_ADDR, 1, 1},

        {MMC_SDHC3_BASE_ADDR, 1, 1},

};

#ifdef CONFIG_DYNAMIC_MMC_DEVNO

int get_mmc_env_devno(void)

{

        uint soc_sbmr = readl(SRC_BASE_ADDR + 0x4);

        return (soc_sbmr & 0x00300000) ? 1 : 0;

}

#endif

#ifdef CONFIG_EMMC_DDR_PORT_DETECT

int detect_mmc_emmc_ddr_port(struct fsl_esdhc_cfg *cfg)

{

        return (MMC_SDHC3_BASE_ADDR == cfg->esdhc_base) ? 1 : 0;

}

#endif

int esdhc_gpio_init(bd_t *bis)

{

        s32 status = 0;

        u32 index = 0;

        u32 cfg = (PAD_CTL_HYS_ENABLE | PAD_CTL_PKE_ENABLE |

                        PAD_CTL_PUE_PULL | PAD_CTL_ODE_OPENDRAIN_NONE |

                        PAD_CTL_DRV_HIGH);

        for (index = 0; index < CONFIG_SYS_FSL_ESDHC_NUM; ++index) {

                switch (index) {

                case 0:

#if 0

                        /*

                        

  • our board haven't this pins

                        

  • with this configuration boot from SD-card success

                         */

                        /* ESDHC1 CD */

                        mxc_request_iomux(MX53_PIN_GPIO_1, IOMUX_CONFIG_ALT6);

                        mxc_iomux_set_pad(MX53_PIN_GPIO_1,

                                        cfg | PAD_CTL_360K_PD);

                        /* ESDHC1 WP */

                        mxc_request_iomux(MX53_PIN_DI0_PIN4, IOMUX_CONFIG_ALT3);

                        mxc_iomux_set_pad(MX53_PIN_DI0_PIN4,

                                        cfg | PAD_CTL_360K_PD |

                                        PAD_CTL_SRE_FAST);

#endif

                        

                        /* ESDHC1 CLK */

                        mxc_request_iomux(MX53_PIN_SD1_CLK, IOMUX_CONFIG_ALT0);

                        mxc_iomux_set_pad(MX53_PIN_SD1_CLK,

                                        cfg | PAD_CTL_100K_PU);

                        /* ESDHC1 CMD */

                        mxc_request_iomux(MX53_PIN_SD1_CMD, IOMUX_CONFIG_ALT0);

                        mxc_iomux_set_pad(MX53_PIN_SD1_CMD,

                                        cfg | PAD_CTL_100K_PU);

                        /* ESDHC1 DAT0 */

                        mxc_request_iomux(MX53_PIN_SD1_DATA0,

                                        IOMUX_CONFIG_ALT0);

                        mxc_iomux_set_pad(MX53_PIN_SD1_DATA0,

                                        cfg | PAD_CTL_100K_PU);

                        

                        /* ESDHC1 DAT1 */

                        mxc_request_iomux(MX53_PIN_SD1_DATA1,

                                        IOMUX_CONFIG_ALT0);

                        mxc_iomux_set_pad(MX53_PIN_SD1_DATA1,

                                        cfg | PAD_CTL_100K_PU);

                        

                        /* ESDHC1 DAT2 */

                        mxc_request_iomux(MX53_PIN_SD1_DATA2,

                                        IOMUX_CONFIG_ALT0);

                        mxc_iomux_set_pad(MX53_PIN_SD1_DATA2,

                                        cfg | PAD_CTL_100K_PU);

                        /* ESDHC1 DAT3 */

                        mxc_request_iomux(MX53_PIN_SD1_DATA3,

                                        IOMUX_CONFIG_ALT0);

                        mxc_iomux_set_pad(MX53_PIN_SD1_DATA3,

                                        cfg | PAD_CTL_100K_PU);

                        /* ESDHC1 LCTL */

                        mxc_request_iomux(MX53_PIN_GPIO_18, IOMUX_CONFIG_ALT6);

                        mxc_iomux_set_pad(MX53_PIN_GPIO_18,

                                        cfg | PAD_CTL_360K_PD);

                        break;

                default:

                        printf("Warning: you configured more ESDHC controller"

                                "(%d) as supported by the board(2)\n",

                               CONFIG_SYS_FSL_ESDHC_NUM);

                        return status;

                }

                status |= fsl_esdhc_initialize(bis, &esdhc_cfg[index]);

        }

        return status;

}

int board_mmc_init(bd_t *bis)

{

        if (!esdhc_gpio_init(bis))

                return 0;

        else

                return -1;

}

#endif

And configuration for booting from NAND:

#define CONFIG_CMD_NAND

#if defined(CONFIG_CMD_NAND)

        #define CONFIG_MXC_NAND

        #define CONFIG_SYS_NAND_MAX_CHIPS     8

        #define CONFIG_SYS_MAX_NAND_DEVICE    1

        #define CONFIG_SYS_NAND_BASE          0x40000000

        #define CONFIG_NAND_FW_16BIT    1 /* 1: 16bit 0: 8bit */

        #define CONFIG_CMD_FLASH

#endif

#if defined(CONFIG_MXC_NAND)

void setup_nand(void)

{

        u32 cfg = (PAD_CTL_PKE_ENABLE | PAD_CTL_PUE_PULL |

                        PAD_CTL_100K_PU | PAD_CTL_ODE_OPENDRAIN_NONE |

                        PAD_CTL_DRV_HIGH);

        clk_config(0, 34, NFC_CLK);

        /* EMI NAND_WEIM_DA[0] */

        mxc_request_iomux(MX53_PIN_EIM_DA0, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA0, cfg);

        /* EMI NAND_WEIM_DA[1] */

        mxc_request_iomux(MX53_PIN_EIM_DA1, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA1, cfg);

        /* EMI NAND_WEIM_DA[2] */

        mxc_request_iomux(MX53_PIN_EIM_DA2, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA2, cfg);

        /* EMI NAND_WEIM_DA[3] */

        mxc_request_iomux(MX53_PIN_EIM_DA3, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA3, cfg);

        /* EMI NAND_WEIM_DA[4] */

        mxc_request_iomux(MX53_PIN_EIM_DA4, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA4, cfg);

        /* EMI NAND_WEIM_DA[5] */

        mxc_request_iomux(MX53_PIN_EIM_DA5, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA5, cfg);

        /* EMI NAND_WEIM_DA[6] */

        mxc_request_iomux(MX53_PIN_EIM_DA6, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA6, cfg);

        /* EMI NAND_WEIM_DA[7] */

        mxc_request_iomux(MX53_PIN_EIM_DA7, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA7, cfg);

        /* EMI NAND_WEIM_DA[8] */

        mxc_request_iomux(MX53_PIN_EIM_DA8, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA8, cfg);

        

        /* EMI NAND_WEIM_DA[9] */

        mxc_request_iomux(MX53_PIN_EIM_DA9, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA9, cfg);

        

        /* EMI NAND_WEIM_DA[10] */

        mxc_request_iomux(MX53_PIN_EIM_DA10, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA10, cfg);

        /* EMI NAND_WEIM_DA[11] */

        mxc_request_iomux(MX53_PIN_EIM_DA11, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA11, cfg);

        /* EMI NAND_WEIM_DA[12] */

        mxc_request_iomux(MX53_PIN_EIM_DA12, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA12, cfg);

        /* EMI NAND_WEIM_DA[13] */

        mxc_request_iomux(MX53_PIN_EIM_DA13, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA13, cfg);

        /* EMI NAND_WEIM_DA[14] */

        mxc_request_iomux(MX53_PIN_EIM_DA14, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA14, cfg);

        /* EMI NAND_WEIM_DA[15] */

        mxc_request_iomux(MX53_PIN_EIM_DA15, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_EIM_DA15, cfg);

        /* EMI NANDF_ALE */

        mxc_request_iomux(MX53_PIN_NANDF_ALE, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_ALE, cfg | PAD_CTL_HYS_ENABLE);

        /* EMI NANDF_CLE */

        mxc_request_iomux(MX53_PIN_NANDF_CLE, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_CLE, cfg | PAD_CTL_HYS_ENABLE);

        /* EMI NANDF_CS[0] */

        mxc_request_iomux(MX53_PIN_NANDF_CS0, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_CS0, cfg | PAD_CTL_HYS_ENABLE);

        /* EMI NANDF_RB[0] */

        mxc_request_iomux(MX53_PIN_NANDF_RB0, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_RB0, cfg | PAD_CTL_HYS_ENABLE);

        /* EMI NANDF_RB_B */

        mxc_request_iomux(MX53_PIN_NANDF_RE_B, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_RE_B, cfg | PAD_CTL_HYS_ENABLE);

        /* EMI NANDF_WE_B */

        mxc_request_iomux(MX53_PIN_NANDF_WE_B, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_WE_B, cfg | PAD_CTL_HYS_ENABLE);

        /* EMI NANDF_WP_B */

        mxc_request_iomux(MX53_PIN_NANDF_WP_B, IOMUX_CONFIG_ALT0);

        mxc_iomux_set_pad(MX53_PIN_NANDF_WP_B, cfg | PAD_CTL_HYS_ENABLE);

}

void setup_nfc(void)

{

        volatile unsigned int reg = 0;

        reg = readl(NFC_BASE_ADDR + 0x24);

        reg &= ~(0x3 << 0);

        reg |= (0x1 << 0);

        writel(reg, NFC_BASE_ADDR + 0x24);

        reg = readl(NFC_BASE_ADDR + 0x28);

        reg &= ~((0x7 << 12) | (0x1 << 3));

        writel(reg, NFC_BASE_ADDR + 0x28);

}

#endif

Sorry for big post.

>

0 项奖励
回复
7,231 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Kirill ,

     I noticed your note on above " with this configuration boot from SD-card success" , what does it mean ?

     Does it mean you can boot the board from SD1 port successfully ?

Regards,

Weidong

0 项奖励
回复
7,231 次查看
BrilliantovKiri
Senior Contributor I

Hello, Weidong!

Yes, system successfully run from SD1, but UART output not work, as I write early.

>

0 项奖励
回复
7,231 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Kirill,

     Please try it in hearder file :

#define CONFIG_MXC_UART  2

Regards,

Weidong

0 项奖励
回复
7,231 次查看
BrilliantovKiri
Senior Contributor I

Hello, Weidong!

I try late, now I havn't hardware, but I think what this is not solve problem because macros CONFIG_MXC_UART only enabled building serial_mxc.

0 项奖励
回复
7,228 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, attached is a i.MX6 BSP porting guide. Chapter 3 is about UART porting. Although it is for i.MX6, the porting is similar to the i.MX53 basically.

0 项奖励
回复
7,228 次查看
BrilliantovKiri
Senior Contributor I

Thank you for your answer, jimmychan!

But I haven't problem in Linux, only in U-Boot and after loading Linux...

U-Boot - I can't get any output after loading from NAND or SD, after loading via MFGToll all ok.

After loading Linux I can't put any commands, but system configured on work with UART2 and I get output from programms, follow my inittab:

::sysinit:/etc/init.d/rcS

::respawn:/sbin/getty -L ttymxc1 115200

::restart:/sbin/init

::ctrlaltdel:/bin/umount -a -r

>

0 项奖励
回复
7,228 次查看
jimmychan
NXP TechSupport
NXP TechSupport

In your U-boot, please try to set CONFIG_CONS_INDEX  to 2 .

Have you set the uart_clk and  early_console_setup in kernel?

For your reference, https://community.freescale.com/message/311767#311767

0 项奖励
回复
7,228 次查看
BrilliantovKiri
Senior Contributor I

Hello, jimmychan!

I try set CONFIG_CONS_INDEX, but this is not solve problem because this define not used in result binary.

As I write early I not have problem with output from Linux.

>

0 项奖励
回复